Skip to main content
FWege.1
Associate II
Jul 20, 2022 11:17 AM UTC
Question

STM32CubeProgrammer STM32G474 option bytes

Dear all

I think the description is wrong or BOOT0/BOOT1 is swapped - see attachments.

If the option bytes are programmed as shown under STM32CubeProgrammer.png, the controller boots from flash.

Thanks in advance,

Franz

This topic has been closed for replies.

1 reply

KiptonM
Senior III
Jul 20, 2022 2:04 PM UTC

Yes they are. I found out the hard way when it did not work. It was pointed out to me to use the documentation (Reference Manual) and that works.