Associate II
December 28, 2022
Solved
STM32CubeProgrammer, STM32G031K8 option bytes problem
- 7 replies
- 3317 views
Hello,
I have NUCLEO-G031K8 and want to change nBOOT0 using STM32CubeProgrammer (v2.12.0) but I'm unable to do so.
I get four message boxes from STM32CubeProgrammer:
- "Warning: Option Byte: nSwap_BANK, does not exist",
- "Warning: Option Byte: DUAL_BANK, does not exist",
- "Warning: option Byte: DUAL_BANK, is not programmable",
- "Option Bytes successfully programmed".
Even though the fourth message box says that option bytes were successfully programmed - nBOOT0 value is unchanged.
Here's log from STM32CubeProgrammer:
09:41:13 : Option byte command : -ob DUAL_BANK=1 nSWAP_BANK=1 IRHEN=1 nBOOT1=1 nBOOT_SEL=1 RAM_PARITY_CHECK=1 WWDG_SW=1 IWDG_STDBY=1 IWDG_STOP=1 IWDG_SW=1 nRST_SHDW=1 nBOOT0=1
09:41:13 : PROGRAMMING OPTION BYTES AREA ...
09:41:13 : Warning: Option Byte: DUAL_BANK, is not programmable
09:41:13 : Warning: Option Byte: DUAL_BANK, does not exist
09:41:13 : Warning: Option Byte: nSWAP_BANK, does not exist
09:41:13 : Bank : 0x00
09:41:13 : Address : 0x40022020
09:41:13 : Size : 108 Bytes
09:41:13 : Reconnecting...
09:41:14 : Reconnected !
09:41:14 : UPLOADING OPTION BYTES DATA ...
09:41:14 : Bank : 0x00
09:41:14 : Address : 0x40022020
09:41:14 : Size : 108 Bytes
09:41:14 : Bank : 0x01
09:41:14 : Address : 0x40022080
09:41:14 : Size : 4 Bytes
09:41:14 : OPTION BYTE PROGRAMMING VERIFICATION:
09:41:14 : Option Bytes successfully programmed
09:41:14 : Time elapsed during option Bytes configuration: 00:00:01.199What's strange I can change nBOOT0 using old, depreciated STM32 ST-LINK Utility (v.4.6.0).
Does anyone have a clue what I'm doing wrong?
Thanks!