Skip to main content
Associate III
Nov 11, 2025 8:01 AM UTC
Question

STM32CUBEprogrammer software bug

This software has too many bugs. Could the developers please look into the main issues? 1. If the downloader fails to connect, it spams dozens of error messages. 2. Frequent freezing, primarily when the downloader fails to connect—the software gets stuck and can't even be closed, which severely impacts usability.
 

5 replies

mbarg.1
Senior III
Nov 11, 2025 8:08 AM UTC

As most of us do not have such problems, please state your OS, sw version, CPU, ram ...

ST Technical Moderator
Nov 11, 2025 8:25 AM UTC

Hello @zhaowhong ,

Please share more data as mentioned by @mbarg.1 also the log file, to help you in your issues.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
zhaowhongAuthor
Associate III
Nov 12, 2025 6:17 AM UTC

When the software is in a connected state, there's an 80% chance it will freeze if the connected device loses power or the downloader becomes loose.

TDK
Nov 12, 2025 2:16 AM UTC

No problems here.

"If you feel a post has answered your question, please click ""Accept as Solution""."
MGogr.1
Senior
Nov 12, 2025 7:09 AM UTC

No issues found on my device.