Skip to main content
JTomp.1
Associate II
Nov 4, 2020 2:34 PM UTC
Solved

STM32CubeProgrammer reports no STM32 target found.

I'm using the P-NUCLEO-STM32WB55 board and programming was working, but it stopped. I didn't change any jumpers, etc. I'm using a USB cable from PC to the ST-LINK connector. The last firmware successfully programmed was the BLE_TransparentMode example.

Log from CubeProgrammer:

10:19:39:114 : STLinkUSBDriver.dll loaded

10:19:39:117 : STLinkUSBDriver.dll loaded

10:19:39:117 : ST-LINK SN : 0671FF303430484257141247

10:19:39:117 : ST-LINK FW : V2J37M26

10:19:39:121 : Board : P-NUCLEO-WB55

10:19:39:124 : Voltage : 3.27V

10:19:39:140 : Error: No STM32 target found!

Any suggestions greatly appreciated!

Thanks in advance.

Jim

This topic has been closed for replies.
JTomp.1
JTomp.1Best answer
Associate II
Nov 4, 2020 2:51 PM UTC

I changed the reset mode from Software to Hardware and it works. Not sure why this works though.

2 replies

JTomp.1
JTomp.1AuthorBest answer
Associate II
Nov 4, 2020 2:51 PM UTC

I changed the reset mode from Software to Hardware and it works. Not sure why this works though.

Cezar
Explorer II
Nov 13, 2020 3:02 PM UTC

I have same issue but hardware reset doesn't solve it for me.

Any idea what I might try?