Skip to main content
Associate
Aug 5, 2024 1:12 PM UTC
Solved

STM32CubeProgrammer issue with West flash command

It's the first time I encounter this issue so I'm not familiar with it. It happens with the command "west flash". The problem started after upgrading Zephyr to v3.6.0. Prior to that it was working. Any hints are appreciated!

usage: stm32cubeprogrammer [-h] [-d DIR] [-r RUNNER] [--skip-rebuild] [--domain DOMAIN] [-H] [--board-dir DIR] [--gdb GDB] [--openocd OPENOCD] [--openocd-search DIR]
 [--elf-file FILE] [--hex-file FILE] [--bin-file FILE] [--erase] [-O TOOL_OPT] --port PORT [--frequency FREQUENCY] [--reset-mode {sw,hw,core}]
 [--conn-modifiers CONN_MODIFIERS] [--cli CLI] [--use-elf]
stm32cubeprogrammer: error: argument --reset/--no-reset: ignored explicit argument 'hw'

xavierpachecoeaton_0-1722863370555.png

 

This topic has been closed for replies.
Sarra.SBest answer
ST Employee
Aug 6, 2024 8:25 AM UTC

Hello @xavierpacheco-eaton, 

Verify if CubeProgrammer is added in the boards\st\xxxxxx\board.cmake after upgrade. If not, add 

board_runner_args(stm32cubeprogrammer "--port=swd" "--reset-mode=hw")
include(${ZEPHYR_BASE}/boards/common/stm32cubeprogrammer.board.cmake)

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

Sarra.SBest answer
ST Employee
Aug 6, 2024 8:25 AM UTC

Hello @xavierpacheco-eaton, 

Verify if CubeProgrammer is added in the boards\st\xxxxxx\board.cmake after upgrade. If not, add 

board_runner_args(stm32cubeprogrammer "--port=swd" "--reset-mode=hw")
include(${ZEPHYR_BASE}/boards/common/stm32cubeprogrammer.board.cmake)

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Employee
Aug 6, 2024 8:01 PM UTC

Hi All,

 

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.

 

Regards,

Jake

ST Support

Associate
Aug 6, 2024 8:21 PM UTC

The issue has been resolved. As @Sarra.S pointed out, I needed to update the following line and replace --reset with --reset-mode. 

board_runner_args(stm32cubeprogrammer "--port=swd" "--reset-mode=hw")

Thank you!