Skip to main content
waclawek.jan
Super User
August 11, 2021
Solved

STM32CubeProgrammer incorrectly displays BKPSRAM content

Below CubeProgrammer's window is gdb displaying the real content of BKPSRAM.

0693W00000D29yVQAR.png 

JW

This topic has been closed for replies.
Mike_ST
Mike_STBest answer
ST Technical Moderator
August 30, 2021

Hello Jan,

Go to memory editor part (the same one you shown on the picture), enter the reg address and write desired reg value.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 

12 replies

Mike_ST
ST Technical Moderator
August 11, 2021

Thank you.

Ticket entered...

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
waclawek.jan
Super User
August 11, 2021

Hi @Mike_ST​ ,

Thanks.

Jan

Mike_ST
ST Technical Moderator
August 26, 2021

Hello Jan,

I got feedback...

It seems like in the GDB setup you are using the BKPSRAM has been activated previously,

When STM32CubeProgrammer is only reading memory without doing activation.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
waclawek.jan
Super User
August 26, 2021

Hi Mike,

What do you mean by *activation* here, in terms of the Reference Manual?

And what should I do to "activate" the BKPSRAM so that it is readable by CubeProgrammer?

Thanks,

Jan

@Mike_ST​ 

Mike_ST
ST Technical Moderator
August 27, 2021

Hi Jan,

RCC.PWREN set to 1

RCC.BKPSRAMEN set to 1

PWR.BDP set to 1

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
waclawek.jan
Super User
August 28, 2021

Hi Mike,

Thanks.

So, how do I set those bits in CubeProgrammer, so that I can read out (and eventually reprogram) content of BKPSRAM?

Thanks,

Jan

@Mike_ST​ 

Mike_ST
Mike_STBest answer
ST Technical Moderator
August 30, 2021

Hello Jan,

Go to memory editor part (the same one you shown on the picture), enter the reg address and write desired reg value.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
waclawek.jan
Super User
August 31, 2021

Hi Mike,

OK, this works. For read, it's enough to set RCC_AHB1ENR.BKPSRAMEN of course.

CubeProgrammer could do this automatically, though, when access to the BKPSRAM area is requested; I don't see any danger stemming from this.

It also could support write in the same manner, besides PWR_CR.DBP perhaps also setting PWR_CSR.BRE (but that should perhaps be optional).

Can this please be chalked up as a feature request to CubeProgrammer? After all, BKPSRAM is a nonvolatile memory, thus similar in usage to FLASH...

Thanks for your support,

Jan

@Mike_ST​ 

Mike_ST
ST Technical Moderator
August 31, 2021

Hi again,

"CubeProgrammer could do this automatically"

Actually I asked for that in the ticket. It has been rejected, because we want to display original memory/register state.

You can try automate the process by creating a batch script that call STM32CubeProgrammer with the w32 command to set the 3 registers.

STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe -c port=SWD mode=normal -w32 0x40023840 0x10000000 -w32 0x40023830 0x00140000 -w32 0x40007000 0x0000C100

Then you have to connect in "Hotplug" mode, not "Normal" or under "Reset".

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
waclawek.jan
Super User
August 31, 2021

Hi Mike,

> It has been rejected, because we don't want to display original memory/register state.

I don't understand what that means, but whatever, I assume this is to keep behaviour consistent which is a good thing.

> You can try automate the process

Thanks for the suggestion.

My original application was to quick-check self-measured calibration data during manufacturing, using the clicky interface; so any "intermediate" step would defeat this particular purpose. I've arranged for a different process meantime.

Thanks again for your involvement.

Jan

@Mike_ST​