Skip to main content
David Littell
Senior II
Nov 10, 2021 2:10 PM UTC
Question

STM32CubeProgrammer getting buggier

2.8.0 doesn't handle multiple ST-LINKs correctly. A new instance of CubeProgrammer usually makes the absolute wrong decision to use an ST-LINK already assigned to another CubeProgrammer instance.

2.8.0 seems to have become more unforgiving with issues on the target processor (being held in reset, etc.) and simply crashes.

This topic has been closed for replies.

8 replies

Houda GHABRI
ST Employee
Nov 19, 2021 1:02 PM UTC

Hi @David Littell​ ,

Let me be sure that I understand the issue, a new instance always select a serial number already assigned and you need that Cubeprogrammer switch to unused one?

This is the default behavior and common to all CubeProgrammer version , user have to to select manually different Serial number :

0693W00000GYCYhQAP.png 

Hope this helps you.

Houda

David Littell
Senior II
Nov 19, 2021 3:12 PM UTC

Yeah, I know what it does. I'm saying what it does is stupid - there's no sane reason for a new instance of CubeProgrammer to by default select an ST-LINK that's already in use by another instance of CubeProgrammer.

Tesla DeLorean
Guru
Nov 19, 2021 10:04 PM UTC

There doesn't seem to be any "Dog Fooding" testing at ST, whereby actual use of the software by the development group, in a real-world sense, would allow for observation of basic bugs, user interface issues, diagnostic reporting and generally annoying behaviour, and fix them immediately.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
RRoma.4
Associate
Nov 20, 2021 1:23 PM UTC

Hello David, I confirm your issue: unconnected processor or simply plugging in an ST-Link (2 for sure, 3 not at hand now) when you hit "connect" crash.

Nov 21, 2021 3:46 PM UTC

What is the reason behind having two programmers connected while working with the cubeProgrammer? I think the use case of cubeProgeammer is in the production line, no other thing.

RRoma.4
Associate
Nov 21, 2021 9:54 PM UTC

Hello, Cube programmer has some feature that help debugging multiprocessor systems.

Example, debugging state on one processor and start stop or reset another processor.

Why? Cube programmer simply can access debug, cube IDE instead reload code wearing flash. Start stop restart just at one button press.

This scenario 3 or more programmer active is not an isolated case.

Flash area patch on the field to change some table of specific processor across cluster... Every node can be accessed and tables changed on the fly.

This Way is not a production dedicated but a powerful debugging and/or tuning instrument.

Save state of program to flash, debugger cannot be used without erasing data so log can be dumped only using cube programmer