Skip to main content
Associate
Apr 16, 2026 3:28 PM UTC
Question

STM32CubeProgrammer for macOS

It would be nice if the further versions could be running on case sensitive file system on macOS.
Currently I need to use an USB key formatted APFS only. Then i can run the installer and install the programmer on this USB stick. As I most of the time only need the command line tools (*CLI) I copied the binaries and some folders with data on my case sensitive disk. They work fine. Only the GUI is not possible on the case-sensitive file system.

 

1 reply

Kouthair
ST Technical Moderator
Apr 30, 2026 3:26 PM UTC

Hello @Laur59 ,

I was able to recreate the same behavior, and I have forwarded your request to our development team to look further into it. (Internal ticket ID: 0062279)

I will let you know if there are any updates on this matter.

PS: Ticket ID: 0062279 is an internal tracking number and is not accessible or usable by customers.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.