Skip to main content
CTapp.1
Senior III
Dec 3, 2024 4:31 PM UTC
Solved

STM32CubeProgrammer fails to program an STM32H7B3I-DK

I have a Touch-GFX project that I can program into an STM32H7B3I-DK from within the STM32CubeIDE.

However, trying to program the same board with the project's .elf file from STM32CubeProgrammer fails with:

16:20:21 : Memory Programming ...
 16:20:21 : File : STM32H7B3I-DK.elf
 16:20:21 : Size : 1.36 MB 
 16:20:21 : Address : 0x08000000 
 16:20:21 : Erasing memory corresponding to segment 0:
 16:20:21 : Erasing internal memory sectors [0 51]
 16:20:21 : Erasing memory corresponding to segment 2:
 16:20:21 : Download in Progress:
 16:20:22 : Error: failed to download Segment[2]
 16:20:22 : Error: failed to download the File

Running at Verbosity Level 3 doesn't add much:

16:21:10:229 : Segment[0] downloaded successfully
 16:21:10:229 : Size : 1013268 Bytes
 16:21:10:229 : Address : 0x90000000 
 16:21:10:229 : Buffer program...
 16:21:10:230 : w ap 0 @0x90000000 : 0x000F7614 bytes, Data 0xE708F0F8...
 16:21:10:230 : Error: failed to download Segment[2]
 16:21:10:230 : Error: failed to download the File
 16:21:10:254 : r ap 0 @0x1FF13FFE 0x00000001 bytes Data 0xFFFFFF92 <-- this line repeats forever

I am using V2.18.0 of the programmer.

Any idea what's causing this?

I need to get the programmer working as people who only need to update the firmware will be using it, and they don't want to have to learn how to use the full IDE.

This topic has been closed for replies.
CTapp.1
CTapp.1Best answer
Senior III
Dec 4, 2024 3:16 PM UTC

The MX25LM51245G_STM32H7B3I-DISCO External Loader is needed to program the system.

It was appearing to work as the erase did not erase the external NOR FLASH, so only the MCU needed to be programmed to get it running (though probably not if the code had changed).

 

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)

2 replies

CTapp.1
CTapp.1Author
Senior III
Dec 4, 2024 9:20 AM UTC

Strangely, it appears as if the programming may actually have worked, even though it is reported as having failed!

The application appears to work correctly if I disconnect the programmer or set it to "Run after programming". I have verified it is programming something by executing a full erase before trying to program to make sure the system would be erased if the programming failed.

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)
CTapp.1
CTapp.1AuthorBest answer
Senior III
Dec 4, 2024 3:16 PM UTC

The MX25LM51245G_STM32H7B3I-DISCO External Loader is needed to program the system.

It was appearing to work as the erase did not erase the external NOR FLASH, so only the MCU needed to be programmed to get it running (though probably not if the code had changed).

 

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)