Skip to main content
JVers.6
Visitor II
Aug 8, 2018 9:42 AM UTC
Question

STM32Cubeprogrammer fails to install in MacOS

When starting install as described in documents, the setup icon appears and disappears directly. I tried to open the installer from the command line and then the following error message appears "LSOpenURLsWithRole() failed with error -10810 for the file /Users/joszelf/Downloads/en/SetupSTM32CubeProgrammer-1.1.0.app. "

Latest version of Java is installed. MacOS Latest version

This topic has been closed for replies.

9 replies

john doe
Senior III
Aug 8, 2018 1:13 PM UTC

these applications need java 8 and wont work with java 10.

also, st does not digitally sign their binaries, so the mac os puts it in quarantine

use the command

xattr -d com.apple.quarantine <the path to your installer>

to remove the quarantine flag

also, dont install as root into /Applications. install it as a normal user into somewhere else, such as Developer. same with the CubeMX application.

ST Technical Moderator
Sep 25, 2018 3:44 PM UTC

Hello @JVers.6​ 

Could you please specify the MAC Os version used?

This issue is raised internally for check and we will come back to you as soon as possible.

Kind Regards,

Imen.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
PMona
Associate
Nov 13, 2018 7:14 PM UTC

Rather than launch the STM32Cube installer app, I selected the app, then Ctrl-Clicked to select "Show Package Contents". Next, Navigate to Contents>>macOs then Ctrl-Click on SetupSTM32CubeProgrammer-1_2_1_macos and select "Open" and the installer will run

ptian
Visitor II
Jul 7, 2020 7:13 PM UTC

Yeah, finally find the correct way to install. Helps me a lot! Thank you!:grinning_face:

whatcall
Visitor II
Dec 21, 2018 4:06 AM UTC

Same issue with running the SetupSTM32CubeProgrammer-1.3.0

The command line running raises error:

➜ SetupSTM32CubeProgrammer-1.3.0.app /Applications/SetupSTM32CubeProgrammer-1.3.0.app/Contents/MacOs/SetupSTM32CubeProgrammer-1_3_0_macos
Error: Unable to access jarfile ../../../SetupSTM32CubeProgrammer-1.3.0.exe

macOS 10.14.2

java -version

java version "1.8.0_121"

Java(TM) SE Runtime Environment (build 1.8.0_121-b13)

Java HotSpot(TM) 64-Bit Server VM (build 25.121-b13, mixed mode)

My previous installed STM32CubeMX app works normally.

KDeli.1
Associate II
Jul 13, 2020 12:44 AM UTC

hello, did you solve your problem? i have the same issue

PMona
Associate
Jul 13, 2020 1:52 AM UTC

My recollection is that I dragged the existing app and associated folders to the trash, then installed.

KDeli.1
Associate II
Jul 13, 2020 7:37 PM UTC

After that the problem still exist, "..failed with error -1081" with the latsest Java edition