Skip to main content
RHine.1
Associate
May 6, 2020 6:44 AM UTC
Question

STM32CubeProgrammer fails to install in 32-bit Linux with the following error Failed to parse: /home/richard/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/libstp11_SAM.so.conf I did not see a solution to the problem

..

This topic has been closed for replies.

4 replies

Imen GH
ST Employee
May 6, 2020 8:55 AM UTC

​Hello,

According to user Manual UM2237 of STM32CubeProgrammer software description , the Supported operating systems and architectures are :

   Linux: 64-bit

   Windows:7/8/10 32-bit and 64-bit

   macOS: (minimum version OS X® Yosemite)

So, it does not support Linux: 32-bit

Regards

RHine.1
RHine.1Author
Associate
May 6, 2020 4:55 PM UTC
1.1 System requirements Supported operating systems and architectures: • Linux® 32-bit and 64-bit (tested on Ubuntu 14.04) • Windows® 7/8/10 32-bit and 64-bit • macOS® (minimum version OS X® Yosemite) The Java™ SE Run Time Environment 1.8 (version 1.8.121 or newer) from Oracle® must be installed. (Download available from www.oracle.com) The minimal supported screen resolution is 1024x768.