Skip to main content
sdanie
Visitor II
Jan 8, 2020 11:21 AM UTC
Question

STM32CubeProgrammer does not start up on Windows (Version 2.2 and 2.3)

Issue:

When I try to start the STM32CubeProgrammer application the splash screen pops up for a short moment but then the application stops immediately.

The CLI variant seems at least it's help dump is functional.

The TrustedPackageCreator application starts up as well.

I tried different ways to solve this issue. Switching between Version 2.2 and 2.3.

Uninstalling the Java SDK. The USB driver seems to work properly. At least the attached STM32 BOOTLOADER is listed in the device manager. My colleagues have a similar setup on their machine and the STM32CubeProgrammer application works properly.

Any advice how to solve this issue or identify the root cause? So far I was not able to find any CrashDumps on my machine.

My environment:

Windows 10 1809 17763.914 (defined by IT policy)

Java(TM) SE Runtime Environment (build 1.8.0_231-b11)

Java HotSpot(TM) 64-Bit Server VM (build 25.231-b11, mixed mode)

No JDK or newer version of Java installed.

Update: It seems to be related to my users profile (Registry, Appdata etc.)

Using a different account the same installation with the same JRE works properly. Any advice or experience with such a behavior?

This topic has been closed for replies.

1 reply

DFlam
Associate
Mar 27, 2020 10:23 AM UTC

I have the same problem with versions 2.2, 2.3 and 2.4.

Only version 2.1 works on my PC.

Any news on how to solve this issue?

thanks,

Davide.