Skip to main content
Associate
Feb 14, 2025 6:21 AM UTC
Question

STM32CubeProgrammer CLI Standalone Version

Hi to all

I just wan't to use the CLI inteface from STM32CubeProgrammer and I don't want to installl the full SMT32CubeProgrammer which is about 1.3GB.

Is there a Standalone Version from the STM32CubeProgrammer CLI?

Best regards

This topic has been closed for replies.

3 replies

TDK
Feb 14, 2025 2:36 PM UTC

There's not a standalone unfortunately, and STM32CubeProgrammer has grown to be a beast. We used to have the relatively lightweight ST-Link Utility, which still works for older chips.

There is the open source st-flash which mostly works but can struggle with newer hardware until development catches up.

stlink-org/stlink: Open source STM32 MCU programming toolset

Think those are your only options.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Pavel A.
Feb 14, 2025 2:58 PM UTC

CubeProgrammer CLI is not just the program itself. (even with all these chubby Qt libraries). It comes with database of MCUs and external loaders. Bottom line: keep it simple, not small.