Skip to main content
Visitor II
Apr 14, 2025 12:02 PM UTC
Question

STM32CubeProgrammer cant use UART in Version 2.19.0

Hello,

I am using the UART-Connection to programm an ST32G431.

With SW 2.5.0 all is fine:

13:10:11 : STM32CubeProgrammer API v2.5.0
13:10:25 : Serial Port COM4 is successfully opened.
13:10:25 : Port configuration: parity = even, baudrate = 115200, data-bit = 8,                     stop-bit = 1.0, flow-control = off
13:10:26 : Activating device: OK
13:10:26 : Chip ID: 0x468
13:10:26 : BootLoader protocol version: 3.1
13:10:27 : UPLOADING OPTION BYTES DATA ...
13:10:27 :   Bank          : 0x00
13:10:27 :   Address       : 0x1fff7800
13:10:27 :   Size          : 36 Bytes
13:10:27 :   Bank          : 0x01
13:10:27 :   Address       : 0x1fff7828
13:10:27 :   Size          : 4 Bytes
13:10:28 : UPLOADING ...
13:10:28 :   Size          : 1024 Bytes
13:10:28 :   Address       : 0x8000000
13:10:28 : Read progress:
13:10:29 : Data read successfully
13:10:29 : Time elapsed during the read operation is: 00:00:01.112
13:14:40 : Disconnected from device.

with SW2.19.0 it goes wrong:

13:14:49 : RTS low
13:14:49 : DTR low
13:14:49 : Serial Port COM4 is successfully opened.
13:14:49 : Port configuration: parity = even, baudrate = 115200, data-bit = 8,                     stop-bit = 1.0, flow-control = off
13:14:49 : Activating device: OK
13:14:49 : Board       : --
13:14:49 : Chip ID: 0x468
13:14:49 : BootLoader protocol version: 3.1
13:14:50 : Response received from device: NACK
13:14:50 : Error: Address not acknowledged: 0x1FFF75E0
13:14:50 : Response received from device: NACK
13:14:50 : Error: Address not acknowledged: 0x1FFF75E0
13:14:50 : Response received from device: NACK
13:14:50 : Error: Address not acknowledged: 0x1FFF75E0
13:14:50 : Error: Database: There's no active configuration for this device. All the 3 configurations are disabled!
13:14:52 : UPLOADING OPTION BYTES DATA ...
13:14:52 :   Bank          : 0x00
13:14:52 :   Address       : 0x1fff7800
13:14:52 :   Size          : 44 Bytes
13:14:52 : UPLOADING ...
13:14:52 :   Size          : 1024 Bytes
13:14:52 :   Address       : 0x8000000
13:14:52 : Read progress:
13:14:53 : Data read successfully
13:14:53 : Time elapsed during the read operation is: 00:00:01.112

I got Error: Database: There's no active configuration for this device. All the 3 configurations are disabled!

and i cant programm the MCU.

What happens?

This topic has been closed for replies.

1 reply

Maryem
ST Employee
Apr 15, 2025 9:38 AM UTC

Hello @FN_it and welcome to the Community,

 

 

Thank you for bringing this to our attention.

A ticket has been submitted to the concerned team to address this issue.

Internal ticket number: 207739 (This is an internal tracking number and is not accessible or usable by customers)

I will keep you updated about any progress.

 

Maryem.

 
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.