Skip to main content
Nawres GHARBI
ST Technical Moderator
Jul 26, 2021 8:55 AM UTC
Question

STM32CubeProgrammer 2.8.0

New features

• Added the support for the STM32U575/585 microcontrollers

• Added the support for SFI via the JTAG interface for the STM32U575/585 microcontrollers

• Added the support for SFI via the bootloader interface (USB/UART/I2C/SPI) for the STM32U5 Series

• Added the new FUS-Operator support for the STM32WB1xxx microcontrollers

• Added the anti-rollback support for the STM32WB1xxx and STM32WB5xxx microcontrollers

• Added the support of FUS version display for the STM32WB1xxx and STM32WB5xxx microcontrollers

• Added the support for the Live Grid Update feature

• Added the support for the Blank check feature

• Added the support for the Memory/File and File/File compare features

• Added the support for the bootloader version display feature

• Added the support for the Fill memory feature

• Added the support for UART interface RTS/CTS signals

• Added the support for Connect while Watchdog enabled

Main issues fixed in STM32CubeProgrammer v2.8.0

  • 64267 Fix issues with FUS via USART boot mode.
  • 72832 Fix issue with MCU ID for STM32L151VB and STM32L151CB.
  • 74327 [STM32F7] Unable to read/write data when option byte WWDG_SW is unchecked.
  • 76440 [STM32WB] Extra bytes are programmed.
  • 81646 STM32G431RB WRP modification.
  • 93987 [STM32G0][GUI] Remove NRST_MODE.
  • 100150 Programming of option bytes list is not completed when SEC_SIZE option byte is programmed.
  • 101017 [STM32H7] Completes data with 00 bytes at the end.
  • 102103 [STM32G0] Bit field for BORR and BORF are swapped.
  • 104089 [STM32G0] Only half of the Flash memory is shown under “Erase & Programming�?, and missing DUAL_BANK and (n)SWAP_BANK option bytes for STM32G0[B-C][0-1]xE microcontrollers.
  • 104320 [STM32WB] The stack “Firmware delete�? button is greyed out when connected through USB DFU.
  • 104707 [STM32U5] RDP regression is not possible when IWDG_SW/WWDG_SW option byte is set to 1.
  • 104832 [STM32G0] NRST_MODE option byte has been removed for STM32G0x1xx microcontrollers.
  • 105628 [STM32U5] HDP option byte is not visible. did
This topic has been closed for replies.

2 replies

_dalbert
Associate II
Oct 4, 2021 5:36 PM UTC

STM32CubeProgrammer v2.8.0 remains seriously broken.

When running with OpenJDK 11 (Azul JDK), 2.8.0 silently fails when programming STM32L471 targets via UART (a subsequent verify shows the failure). This is 100% reproducible. I've been reporting serious flash programming bugs for these targets for nearly a year (since 2.5.0) (ref. case 00135468 and see also STM32CubeProgrammer is not able to successfully connect to or flash an STM32L471. This is a long-standing problem. I have no problem flashing other STM32L parts such as L051 and I have no problem flashing the L471 using an STLinkv2.)

Are there plans to fix STM32CubeProgrammer? Is there an alternate solution?

MChan.5
Visitor II
Oct 16, 2021 7:21 PM UTC

Installer for MacOS version cannot start at all. Even some hack to start, there is error to copy JRE. And no way to start the programmer at all. This problem exists for more than half year.