Skip to main content
ESore.2
Associate
Jul 15, 2021 9:09 AM UTC
Question

STM32CubeProgrammer (2.7.0) screen get corrupted. Any ideas ?

After PC boot program works fine for some time but after some time the screen is corrupted.

(also seen a completely black or a completely white screen). When clicking the pop-up windows are however OK.

This topic has been closed for replies.

3 replies

ST Technical Moderator
Jul 26, 2021 3:21 PM UTC

Hello @ESore.2​ and welcome to the Community :)

Please use the new release STM32CubeProgrammer 2.8.0 available in the ST web site.

Then, please keep me informed about your update.

If your issue is solved, please mark my answer as best by clicking on the "Select as Best" button. This will help other users find this solution more quickly.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
Jul 31, 2021 9:51 PM UTC

Hi @ESore.2​ ,

Please share your update and let me know if your issue is solved with latest release of CubeProgrammer.

Thanks

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ESore.2
ESore.2Author
Associate
Sep 15, 2021 7:41 AM UTC

Finally I managed to update to version 2.8.0 - unfortunately the problem persists :|

I managed to see a message which was showed for a very short moment and only one time when trying to start the program

The message was something like "OpenJDP Platform binary not responding" and was in local language (so probably a windows generated message)

After a PC reboot the STM32CubeProgrammer 2.8.0  always start. If start fails it may restart after a number of retries.

In some cases it seems like the although the screen is blank, the program still reacts on mouse clicks.

Could the reason for the problem be that the OpenJDP Platform binary software does not work stable on my PC*

*) HP ProBook 470 with Intel HD Graphics 4600 / Windows 10