Question
STM32CubeProgrammer 2.6.0 does not launch on OSX (11.1, Big Sur)
Launching the app from the bin directory doesn't work either and there are no errors in the terminal. It just silently fails. I believe part of the problem is the update to version 2.6.0 which uses its own bundled JRE. Perhaps there is a conflict with the OpenJDK (Amazon Corretto) JRE installed on my machine. However, it is necessary to have JRE on my machine to run STM32CubeMX and STM32CubeIDE.
I tried to download the previous version (2.5.0) and run that. It does not launch either, however, there are errors in the terminal.
~ % /Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app/Contents/MacOs/bin/STM32CubeProgrammer ; exit;
Exception in Application start method
java.lang.reflect.InvocationTargetException
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at com.sun.javafx.application.LauncherImpl.launchApplicationWithArgs(LauncherImpl.java:389)
at com.sun.javafx.application.LauncherImpl.launchApplication(LauncherImpl.java:328)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at sun.launcher.LauncherHelper$FXHelper.main(LauncherHelper.java:873)
Caused by: java.lang.RuntimeException: Exception in Application start method
at com.sun.javafx.application.LauncherImpl.launchApplication1(LauncherImpl.java:917)
at com.sun.javafx.application.LauncherImpl.lambda$launchApplication$1(LauncherImpl.java:182)
at java.lang.Thread.run(Thread.java:748)
Caused by: javafx.fxml.LoadException:
file:/Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app/Contents/MacOs/bin/STM32CubeProgrammer!/fxml/MainWindow.fxml:217
at javafx.fxml.FXMLLoader.constructLoadException(FXMLLoader.java:2601)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:2579)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:2441)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:3214)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:3175)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:3148)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:3124)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:3104)
at javafx.fxml.FXMLLoader.load(FXMLLoader.java:3097)
at com.st.app.Main.start(Main.java:38)
at com.sun.javafx.application.LauncherImpl.lambda$launchApplication1$8(LauncherImpl.java:863)
at com.sun.javafx.application.PlatformImpl.lambda$runAndWait$7(PlatformImpl.java:326)
at com.sun.javafx.application.PlatformImpl.lambda$null$5(PlatformImpl.java:295)
at java.security.AccessController.doPrivileged(Native Method)
at com.sun.javafx.application.PlatformImpl.lambda$runLater$6(PlatformImpl.java:294)
at com.sun.glass.ui.InvokeLaterDispatcher$Future.run(InvokeLaterDispatcher.java:95)
Caused by: java.lang.RuntimeException: java.lang.reflect.InvocationTargetException
at javafx.fxml.JavaFXBuilder$ObjectBuilder.build(JavaFXBuilderFactory.java:278)
at javafx.fxml.FXMLLoader$ValueElement.processEndElement(FXMLLoader.java:763)
at javafx.fxml.FXMLLoader.processEndElement(FXMLLoader.java:2823)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:2532)
... 14 more
Caused by: java.lang.reflect.InvocationTargetException
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at sun.reflect.misc.Trampoline.invoke(MethodUtil.java:72)
at sun.reflect.GeneratedMethodAccessor1.invoke(Unknown Source)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at sun.reflect.misc.MethodUtil.invoke(MethodUtil.java:276)
at javafx.fxml.JavaFXBuilder$ObjectBuilder.build(JavaFXBuilderFactory.java:270)
... 17 more
Caused by: java.lang.UnsatisfiedLinkError: Can't load library: /Library/Java/JavaVirtualMachines/amazon-corretto-8.jdk/Contents/Home/jre/lib/libjfxwebkit.dylib
at java.lang.ClassLoader.loadLibrary(ClassLoader.java:1820)
at java.lang.Runtime.load0(Runtime.java:810)
at java.lang.System.load(System.java:1088)
at com.sun.glass.utils.NativeLibLoader.loadLibraryFullPath(NativeLibLoader.java:201)
at com.sun.glass.utils.NativeLibLoader.loadLibraryInternal(NativeLibLoader.java:94)
at com.sun.glass.utils.NativeLibLoader.loadLibrary(NativeLibLoader.java:39)
at com.sun.webkit.WebPage.lambda$static$0(WebPage.java:133)
at java.security.AccessController.doPrivileged(Native Method)
at com.sun.webkit.WebPage.<clinit>(WebPage.java:132)
at javafx.scene.web.WebEngine.<init>(WebEngine.java:881)
at javafx.scene.web.WebEngine.<init>(WebEngine.java:868)
at javafx.scene.web.WebView.<init>(WebView.java:273)
at javafx.scene.web.WebViewBuilder.build(WebViewBuilder.java:60)
... 27 more
Exception running application com.st.app.Main