Skip to main content
Nawres GHARBI
ST Technical Moderator
Feb 26, 2020 9:37 AM UTC
Question

STM32CubeProgrammer 2.4.0 released

New features

• Added the support of the graphic user interface (GUI) for the firmware upgrade service (FUS) and stack upgrade for the entire STM32WB Series

• Support of HSM V2 on all STM32 microcontrollers and microprocessors supporting SFI/SSP

Fixed issues

77015 STM32CubeProgrammer cannot connect ST-LINK without the mass storage feature. 78350 STM32CubeProgrammer issue with STM32G0 when programming binary (size 18448 bytes).

Known problems and limitations

• For the STM32L5 Series, the connection via the ST-LINK protocol is allowed only when mode is set to hotplug with TZEN=1.

• For the STM32L5 Series, the Option Byte programming GUI is not intuitive enough. Refer to the STM32L552xx and STM32L562xx advanced Arm®-based 32-bit MCUs reference manual (RM0438) for permitted accesses.

• For STM32L4Pxxx and STM32L4Qxxx devices, Option Byte programming via bootloader interfaces presents some limitations.

• For STM32H7Axxx and STM32H7Bxxx devices, Option Byte programming via bootloader interfaces (USB) presents some limitations.

• STM32L5 series programming presents limitation in macOS® when TZEN=1 and RDP=0x55.

• With some small-screen resolutions, the graphical interface of STM32CubeProgrammer presents anomalies such as inaccessible buttons.

• Display issues depending on the monitor used can occur with Linux®.

• SFIx on STM32H743/753 devices fails via the debug interface.

• SFI-HSM V2 get certificate fails with STM32L462xx devices.

• Parallel Flash programming fails in macOS® for microprocessors in the STM32MP1 Series

Link:

https://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-programmers/stm32cubeprog.html#overview

This topic has been closed for replies.

12 replies

Uwe Bonnes
Chief
Feb 26, 2020 9:44 AM UTC

Is there a way to update from inside STM32CubeProgrammer?

berendi
Principal
Feb 26, 2020 9:53 AM UTC
waclawek.jan
Super User
Feb 26, 2020 1:18 PM UTC

Does it come with embedded JRE, both the installer and the runtime?

https://community.st.com/s/question/0D70X00000763nW/oracle-jre-license-impact

JW

MHoss.1
Associate III
May 4, 2020 3:47 PM UTC

Unfortunately the new version still does not work with the current Mac OS, returning "LSOpenURLsWithRole() failed with error -10810". I need STM32_Programmer_CLI

but it is not in the app file so I cannot copy it either. Using "java -jar .exe" also does not make the programmer_CLI in the Applications (it has STM32MP_SigningTool_CLI). I'm trying to port SBSFU for my MCU and it seems the scripts need this tool.

Andrei Chichak
Lead
Jun 2, 2020 5:11 AM UTC

June 1st.

Go to the STM32CubeProg home page and you can download versions 2.2.0 or 2.3.0, but not 2.4.0.

Andrei Chichak
Lead
Jun 2, 2020 5:13 AM UTC

Ignore. Human interface fail on my part.

SVogl.1
Associate
Jul 7, 2020 12:18 PM UTC

On MacOS Catalina (10.15.5) the installer does not run because it is unverified; after manual install (java -jar S*.exe), the STM32CubeProgrammer UI refuses to run with 'java.lang.NoClassDefFoundError: javafx/application/Application'

What's missing here?

berendi
Principal
Jul 7, 2020 12:21 PM UTC

> What's missing here?

A well defined release process including test plan.

DWWol.1
Visitor II
Jul 7, 2020 12:40 PM UTC

Greetings.

When to expect a version for Java 11?

On Ubuntu 20.04 with the 8 version of the problem

Joerg Wagner
Senior III
Jul 16, 2020 3:43 PM UTC

Hello.

I use STM32CubeProgrammer 2.4.0 on MacOS Mojave (10.14.6).

No ST-Link is detected. I tried 3 different NUCLEO-F767I (one new board).

A long time ago I had no problems with version 2.1.0.

I can do nothing, no board access and no firmware upgrade.

What is missing or wrong?

Joerg

Joerg Wagner
Senior III
Jul 16, 2020 3:48 PM UTC

Same problem with version 2.2.0 of STM32CubeProgrammer.

Joerg Wagner
Senior III
Jul 17, 2020 2:18 PM UTC

The problem was the USB cable. One data line has a defect probably.