Senior
Mar 23, 2024 10:32 PM UTC
Solved
STM32CubeProgrammer 2.16.0 fails to program STM32L433CC via USB
- 6 replies
- 2951 views
Our customer attempted to update the firmware on their device which uses an STM32L433CC. Programming failed to erase and download the firmware on the device. STM32CubeProgrammer 1.4.0 succeeded in programming the device.
Customer is using a Windows 11 machine with STM32CubeProgrammer 2.16.0.
I have verified that the break occured somewhere between 2.14.0 and 2.16.0 as 2.13.0 works. I have also verified that the behavior is both OS-independent and GUI-independent as I experience the same failure on Linux with 2.16.0 STM32_Programmer_CLI.
This is clearly not a hardware issue, but something wrong with the DFU implementation in STM32CubeProgrammer 2.16.0.
A log file from the failure on Linux is attached.