Skip to main content
FWege.1
Associate II
Jul 20, 2022 9:48 AM UTC
Question

STM32CubeProgrammer 2.11 64Bit setup under Windows 11

Dear all

Under windows 11 the 64 bit setup (2.11) starts

with extracting the file and after that I see sometimes the busy signal, but

...

There are no entries in the windows event logger.

I know, that windows 11 isn’t mentioned in the release notes (RN0109).

Can I start the setup with command line parameters?

Thanks in advance,

Franz

This topic has been closed for replies.

4 replies

FWege.1
FWege.1Author
Associate II
Aug 18, 2023 4:02 PM UTC

The problem still exists with version 2.14.0.

Any assistance would be greatly appreciated.

Pavel A.
Aug 18, 2023 6:37 PM UTC

@FWege.1 What are the missing entries in the Windows event logger? What exactly is the problem? What is the "but..." ?

 

FWege.1
FWege.1Author
Associate II
Aug 18, 2023 10:03 PM UTC

Hello Pavel A.

First - thanks for your answer!

After double clicking the setup file the blue circle (appearing next to the mouse pointer) blinks.
I suppose this indicates some background activity.
Nothing further happens.
The task manager shows 2 processes.

No entry in the windows event log which indicates an error.

Firewall was disabled. Run as administrator was done.

Other installations run as expected.

Pavel A.
Aug 19, 2023 11:02 AM UTC

This is strange, we have installed previous STM32CubeProgrammer versions on Win11 x64 several times and it works well.

Windows is a complex environment with possible presence of 3rd party software and hardware. Troubleshoot as usual for such issues.