Skip to main content
Nawres GHARBI
ST Technical Moderator
Jul 1, 2022 8:47 AM UTC
Question

STM32CubeProgrammer 2.11.0 released

New features

• Tool updater: can be used to upgrade STM32CubeProg from v2.10.0 to v2.11.0 for all supported operating systems (Windows®, Linux®, and macOS®)

• SFI: – SFIx support for STM32U585xx microcontrollers via SWD/JTAG – New SFI/SFIx graphical user interface (GUI) – STM32 Trusted Package Creator SFI GUI enhancement – Support for integrity check with the STM32H7 Series and STM32U5 Series microcontrollers • STM32U5 Series: the GUI supports the RDP regression with password

• New bootloader support for STM32L476xx microcontrollers

• STM32MP13xx microprocessors: – Flash memory load via USB-DFU/UART – SSP (command-line interface only) – OTP: CLI/GUI 

Fixed issues

90858 [STM32WB][CLI] Optimize FUS, STACK, and USER app upgrading automatically. 104409 STM32H735xx: SFI is very slow over SWD.

109240 Extra option bytes displayed for STM32G030C6: PCROP1A_STRT, PCROP1A_END, PCROP1A_RDP, PCROP1B_STRT, PCROP1B_END, and BOOT_LOCK, SEC_SIZE.

110205 Fix the reading of CHIPID (DBGMCU_DBG_AUTH_DEVICE) on STM32U5 microcontrollers.

110614 [CLI] Error level not reported correctly for the CRC safety feature using STM32CubeProgrammer_CLI.

117163 Launch problem when running the STM32CubeProgrammer GUI from another path.

119604 [STM32G0][OB] Sector erase cannot be achieved and an STM32CubeIDE debug error occurs when nSWAP_BANK=0.

120935 STPC v2.9 cannot generate a correct .sfi file for SFI.

121452 [OB] Incorrect SRAM2b secure address for STM32WB1xxx.

121713 Typo: “Memory & file edition�?.

123018 [STM32H7][CM4] BOOT_CM4_ADD cannot be modified.

123740 [DFU] The single-bank configuration is not correctly managed when connecting with DFU.

123913 [CLI] It is not possible to write the LOCK byte.

123923 [UART] A timeout error occurs while disabling the readout protection.

124081 Odd behavior in the log when connecting a NUCLEO-F030R8 using the GUI.

124446 Request to add documentation for the getAuthID command.

124763 [OB] Wrong description of nBOOT1.

125039 [DFU] Strange behavior when trying to program in single-bank mode.

127099 [STM32L4+] Fail to program STM32L4+ twice in a row.

127311 The tool closes automatically when trying to load a file the path of which contains Chinese characters.

127978 Typo in option bytes: IWGDSTDBY. 

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
Jul 1, 2022 12:25 PM UTC
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Peter BENSCH
ST Technical Moderator
Jul 1, 2022 1:57 PM UTC

In case anyone is wondering: there is unfortunately still a typo in the name in the URL (...-v2100-...), but it refers to the correct and current revision 20 of RN0109 for 2.11.0.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
Jul 1, 2022 2:05 PM UTC

@Nawres GHARBI​  thank you to you and Programmer and Loaders team(s)..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
RVoel
Associate
Nov 18, 2022 10:32 AM UTC

I still have problems with the STM32 Programmer in DFU Mode! The programming is running through with a verify error and the controller still has the old programm? See LOG from the programmer!

 11:29:32 : USB speed  : Full Speed (12MBit/s)

 11:29:32 : Manuf. ID  : STMicroelectronics

 11:29:32 : Product ID : STM32 DownLoad Firmware Update

 11:29:32 : SN     : 206130A74734

 11:29:32 : DFU protocol: 1.1

 11:29:32 : Board    : --

 11:29:32 : IAP

 11:29:34 : UPLOADING ...

 11:29:34 :  Size     : 1048576 Bytes

 11:29:34 :  Address    : 0x8000000

 11:29:34 : Read progress:

 11:29:35 : Data read successfully

 11:29:35 : Time elapsed during the read operation is: 00:00:02.450

 11:29:47 : Memory Programming ...

 11:29:47 : Opening and parsing file: STM32L476_DFU.hex

 11:29:47 :  File     : STM32L476_DFU.hex

 11:29:47 :  Size     : 106.77 KB 

 11:29:47 :  Address    : 0x08000000 

 11:29:47 : Erasing memory corresponding to segment 0:

 11:29:47 : erasing sector 0000 @: 0x08000000 done

 11:29:47 : erasing sector 0001 @: 0x08004000 done

 11:29:47 : erasing sector 0002 @: 0x08008000 done

 11:29:47 : erasing sector 0003 @: 0x0800c000 done

 11:29:47 : erasing sector 0004 @: 0x08010000 done

 11:29:47 : Download in Progress:

 11:29:48 : File download complete

 11:29:48 : Time elapsed during download operation: 00:00:00.481

 11:29:48 : Verifying ...

 11:29:48 : Read progress:

 11:29:48 : Error: Data mismatch found at address 0x08000400 (byte = 0xB0 instead of 0xC0)

 11:29:48 : Error: Download verification failed

 11:29:48 : RUNNING Program ... 

 11:29:48 :  Address:   : 0x08000000

 11:29:48 : Start operation achieved successfully

 11:29:48 : Warning: Connection to USB device is lost

 11:29:48 : Disconnected from device.