Skip to main content
Gianluca Costa
Associate II
Jul 7, 2022 7:24 AM UTC
Solved

STM32CubeProgrammer 2.10.0 and 2.11.0 External loader bug: if the EL's filename has more tha one dot (one dot only for its extension name) STM32CubeProgrammer goes in error.

If the name (filename) of module has more than one dot ( "." ) the STM32CubeProgrammer can list it in the external loder (EL) selection, but when STM32CubeProgrammer tries to use the module it fails (it generates an error).

For example this EL name generates the error: EN25Q40_MT447R2_2.0.0.stldr

the same file renamed into EN25Q40_MT447R2.stldr (removing all dots) works.

This topic has been closed for replies.
Houda GHABRI
Houda GHABRIBest answer
ST Employee
Jul 12, 2022 2:57 PM UTC

Hello @Gianluca Costa,

STM32CubeProgrammer should accept more than one dot in EL file name.

I will raise this issue internally to fix it in future release.

Internal ticket number: 131762 (PS: This is an internal tracking number and is not accessible or usable by customers). 

Houda

2 replies

Andrew Neil
Super User
Jul 7, 2022 9:52 AM UTC

Always best to avoid any "weirdness" in file (including folder) names

It's an age-old problem:

https://www.avrfreaks.net/comment/1844411#comment-1844411

https://www.avrfreaks.net/comment/2048571#comment-2048571

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Houda GHABRI
Houda GHABRIBest answer
ST Employee
Jul 12, 2022 2:57 PM UTC

Hello @Gianluca Costa,

STM32CubeProgrammer should accept more than one dot in EL file name.

I will raise this issue internally to fix it in future release.

Internal ticket number: 131762 (PS: This is an internal tracking number and is not accessible or usable by customers). 

Houda