Skip to main content
RDos
Associate II
Jun 28, 2019 1:14 PM UTC
Question

STM32CubeProg install Ubuntu 18.04

STM32Cube Prog does not work on ubuntu 18.04

Appears to install the openjfx package. Which is already installed

in the java package 11.03

This topic has been closed for replies.

6 replies

roland van straten
Associate III
Jul 2, 2019 10:01 PM UTC

I have the same problem (and many other people) with ubuntu 19.04. The STMCubeProgrammer software has a flaw and it already cost me a lot of time trying to figure out what is happening than could be better spend on developing with the STM32MP1 :-(.

Also see this post that points to the real problem:

`https://askubuntu.com/questions/1153142/openjdk-detected-after-uninstall`

SO PLEASE ST SOLVE THIS PROBLEM ASAP.

joemccarr
Associate III
Aug 10, 2019 3:19 PM UTC

Same here. Linux, the red-headed step child

Fix the damn thing or don't release it.

MJiao
Visitor II
Aug 20, 2019 2:35 AM UTC

same issue here.

MJiao
Visitor II
Aug 20, 2019 1:20 PM UTC

I solved this problem by the following steps:

  • install openjfx from ubuntu official repository
  • switch the java version to openjdk-11 by command line
sudo update-alternatives --config java
  • add javafx modules, --module-path and --add-modules are not supported by openjdk-8, so we have to switch to openjdk-11 to perform this operation, after modules added, we will switch java version back to 8.
java --module-path /usr/share/openjfx/lib --add-modules=javafx.base,javafx.controls,javafx.fxml,javafx.graphics,javafx.media,javafx.swing,javafx.web
  • use first command to switch java version back to openjdk-8

after those steps, I opened the eclipse app, I am not sure was this action fixed anything.

anyway, the stm32cubeprog suddenly worked!

my system config: ubuntu 18.04 lst, openjdk-8, openjdk-11, stm32cubeprog 2.1.0

joemccarr
Associate III
Aug 21, 2019 1:13 AM UTC

Didn't work for me but glad you got it going. I am using the command Line interface option that ST has, that is working.

RNaid.1
Visitor II
Mar 2, 2020 5:40 AM UTC

@MJiao​  its working for me on Mac (in Virtual Machine) using the following commands. Thank You.

  1. sudo apt-get install openjfx
  2. sudo apt-get install openjdk-11-jre
  3. sudo apt-get update
  4. sudo apt-get upgrade
  5. Double Click on the SetupSTM32CubeProgrammer-2.3.0.linux
  6. Done