Skip to main content
Associate
Feb 8, 2026 11:53 PM UTC
Solved

STM32CubeController doesn't recognize STM32f3348-discovery

When I open STM32CubeProgrammer (v2.21.0) it displays an error modal "Old ST-LINK firmware version. Upgrade ST-LINK firmware. 

If I click the "Firmware Upgrade" button an STLinkUpgrade 3.16.8 shows up with 

Current firmware: (blank)

Type: (blank)
Version: Unknown
Update to Firmware: Unknown.

The upgrade button does nothing when clicked. How do I fix this?

I downloaded the software here  https://www.st.com/en/development-tools/stsw-link007.html
After running
/usr/lib/jvm/java-17-openjdk-amd64/bin/java -jar stsw-link007-v3-17-10/stsw-link007/AllPlatforms/STLinkUpgrade.jar

There is another upgrade dialog with version 3.17.10 displaying the same firmware info as above, with the upgrade button greyed out.

Other commands ive run

$ ls -l /dev/bus/usb/001/019
crw-rw----+ 1 root plugdev 189, 18 Feb 9 09:36 /dev/bus/usb/001/019


$ lsusb | grep ST
Bus 001 Device 019: ID 0483:374b STMicroelectronics ST-LINK/V2.1

$ STM32_Programmer_CLI -l
-------------------------------------------------------------------
STM32CubeProgrammer v2.21.0
-------------------------------------------------------------------

===== DFU Interface =====

No STM32 device in DFU mode connected

===== J-Link Interface =====
No J-Link/flasher probe detected.
===== STLink Interface =====
Error: Old ST-LINK firmware version. Upgrade ST-LINK firmware

-------- Connected ST-LINK Probes List --------

ST-Link Probe 0 :
ST-LINK SN : 066DFF545054897087211137
ST-LINK FW : V2J27M15
Access Port Number : 4
Board Name :
-----------------------------------------------

===== UART Interface =====

Total number of serial ports available: 33

Error: Old ST-LINK firmware version. Upgrade ST-LINK firmware
Board Name :
ST-LINK SN: 066DFF545054897087211137
Port: ttyACM0
Location: /dev/ttyACM0
Description: STM32 STLink
Manufacturer: STMicroelectronics

$ls /etc/udev/rules.d/ | grep stlink
49-stlinkv1.rules
49-stlinkv2-1.rules
49-stlinkv2.rules
49-stlinkv3.rules
99-stlink.rules

$ cat /etc/udev/rules.d/49-stlinkv2-1.rules
# stm32 nucleo boards, with onboard st/linkv2-1
# ie, STM32F0, STM32F4.

SUBSYSTEMS=="usb", ATTRS{idVendor}=="0483", ATTRS{idProduct}=="374b", \
MODE="660", GROUP="plugdev", TAG+="uaccess", ENV{ID_MM_DEVICE_IGNORE}="1", \
SYMLINK+="stlinkv2-1_%n"

SUBSYSTEMS=="usb", ATTRS{idVendor}=="0483", ATTRS{idProduct}=="3752", \
MODE="660", GROUP="plugdev", TAG+="uaccess", ENV{ID_MM_DEVICE_IGNORE}="1", \
SYMLINK+="stlinkv2-1_%n"

 



mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Feb 10, 2026 5:19 PM UTC

Hello,

As it's an old device (I assume containing a very old ST-LINK firmware), try to use ST-LINK utility (an old tool) to update your STLINK device using that menu:

mALLEm_0-1770744087274.png

I remember I had same issues with ST-LINK having old firmwares, I solved that with ST-LINK Utility.

After updating the ST-LINK with STLINK utility, then update the device with CubeProgrammer.

Hope that helps.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

3 replies

ST Technical Moderator
Feb 10, 2026 7:08 AM UTC

Hello @elsueno ,

Verify USB recognition and permissions. Check also physical connections and jumper.

Does the problem occur when you use another board, different USB port and new cables?

How to solve connection errors when connecting and programming the STM32 target board

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
elsuenoAuthor
Associate
Feb 10, 2026 7:55 AM UTC
Hello. The cables and connections are all good. I have been
writing/flashing successfully with rust and has all been working well.

What do you mean check the usb permissions? what should they be?
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Feb 10, 2026 5:19 PM UTC

Hello,

As it's an old device (I assume containing a very old ST-LINK firmware), try to use ST-LINK utility (an old tool) to update your STLINK device using that menu:

mALLEm_0-1770744087274.png

I remember I had same issues with ST-LINK having old firmwares, I solved that with ST-LINK Utility.

After updating the ST-LINK with STLINK utility, then update the device with CubeProgrammer.

Hope that helps.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.