Skip to main content
dtarrago
Associate III
Mar 13, 2024 12:41 PM UTC
Question

STM32CUbe programmer v2.15.0

I have detected a problem with the v2.15.0 (64 bits) when flashing a STM32L475 MCU.

The message 'sector nnn does not exist' appears repeatdly when erasing sectors when flashing the device.

This only happens with v2.15.0., and then the device last a lot to be flashed and if there were some preserved flash areas, they are erased 

Nevertheless, if v2.14.0 is used, the update procedure is completely carried out.

So, which is the problem? Is this issue already identified?

 

dtarrago_0-1710333473140.png

 

This topic has been closed for replies.

1 reply

Amine_Jridi
ST Technical Moderator
May 7, 2024 3:47 PM UTC

Hello @dtarrago,

Sorry for the delay. The issue with erasing sectors is a known and our development team is currently addressing it internally ticket: 176977. For the flashing time concerns, the issue is already fixed, I suggest using the latest version, STM32CubeProgrammer v2.16.0. 

Amine

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.