Skip to main content
MRemm.1
Associate
Feb 9, 2022 4:56 PM UTC
Solved

STM32Cube IDE Error: Download verification failed (data mismatch)

I've been using a STM32U585 Discovery kit for a few days and have succesfully run several programs on it. However today I suddenly got this error in STM32CubeIDE when trying to run a new program:

---------------------------------------------------------------------------------------------------------------

Error: Data mismatch found at address 0x0800899C (byte = 0x31 instead of 0x33)

Error: Download verification failed

---------------------------------------------------------------------------------------------------------------

Trying to upload different programs gave the same result, but with the mismatch at different addresses.

Using STM32CubeProgrammer I can erase the flash completely and then normally upload and run code with CubeIDE once, but after uploading a different program again I will get the same error.

I've upgraded the ST Link firmware, no change.

I would appreciate any help in finding the problem as I don't want to use CubeProgrammer to fully erase flash every time.

This topic has been closed for replies.
MRemm.1
MRemm.1Best answer
Associate
Feb 10, 2022 9:11 AM UTC

It seems an option byte was somehow switched.

0693W00000JPG3qQAH.pngI tried different combinations of SWAP_BANK and DBANK and this is what works for me now.

Hopefully this will help someone with the same problem.

1 reply

MRemm.1
MRemm.1AuthorBest answer
Associate
Feb 10, 2022 9:11 AM UTC

It seems an option byte was somehow switched.

0693W00000JPG3qQAH.pngI tried different combinations of SWAP_BANK and DBANK and this is what works for me now.

Hopefully this will help someone with the same problem.