Skip to main content
Associate
Jul 24, 2024 7:46 AM UTC
Solved

STM32 programming via USB

I am programming USB DFU in stm32f407g disc1 but i am not able to connect it in stm32cubeprogrammer as it is showing usb port as usb1. Can anyone tell me is it anything missing?

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jul 24, 2024 8:11 AM UTC

Hello,

How did you proceed? Did you pull the BOOT0 pin to VDD then reset the MCU before to connect?

SofLit_0-1721808402492.png

By default SB18 is soldered pulling down Boot pin to the ground which don't allow you to enter the system bootloader.

You need to unsolder SB18 and and handle BOOT0 externally from the board's pin VDD (system bootloader) and GND (User application).

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

4 replies

AScha.3
Super User
Jul 24, 2024 7:53 AM UTC

And what happens, if using this usb1 ?

If you feel a post has answered your question, please click on " Best Answer ".
Associate
Jul 24, 2024 7:56 AM UTC

if I connects usb1 and click on read , it is not connected and data also not reading. It is showing not connected at top right.

AScha.3
Super User
Jul 24, 2024 8:08 AM UTC

And BOOT0 is hi , at power up /reset ?

If you feel a post has answered your question, please click on " Best Answer ".
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jul 24, 2024 8:11 AM UTC

Hello,

How did you proceed? Did you pull the BOOT0 pin to VDD then reset the MCU before to connect?

SofLit_0-1721808402492.png

By default SB18 is soldered pulling down Boot pin to the ground which don't allow you to enter the system bootloader.

You need to unsolder SB18 and and handle BOOT0 externally from the board's pin VDD (system bootloader) and GND (User application).

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.