Skip to main content
JBond.1
Senior
Sep 11, 2021 10:43 AM UTC
Solved

STM32 IAP bootliader does not work with user application >50kb

Hi, I have STM32F407VET6 with a bootloader which reads microSD card, checks for user application update, flashes if it exist and jumps to use application 0x08004000.

All was working fine when my user application was <48kb. I wrote some additional code (which should not impact the start of the application), and now id does not work.

Previously debbugging started at "HAL_Init()" like it should when user application was <48kb

0693W00000DmsMdQAJ.png 

But now, when user application is >50kb it starts debugging at some kind of wrong address:

0693W00000DmsNMQAZ.png It does not hit "HAL_Init()" anymore like it should.

Why user application size could impact that? Or it could be some kind of different issue?

How could I fix this?

This topic has been closed for replies.
TDK
TDKBest answer
Sep 11, 2021 1:29 PM UTC

Use STM32CubeProgrammer to verify the contents of the flash. If they match, the error is in your program and not the bootloader. Otherwise, the bug is in your program. You can step through to see where it goes wrong, possibly the stack is overwritten, or a memory allocation fails.

"If you feel a post has answered your question, please click ""Accept as Solution""."

12 replies

TDK
TDKBest answer
Sep 11, 2021 1:29 PM UTC

Use STM32CubeProgrammer to verify the contents of the flash. If they match, the error is in your program and not the bootloader. Otherwise, the bug is in your program. You can step through to see where it goes wrong, possibly the stack is overwritten, or a memory allocation fails.

"If you feel a post has answered your question, please click ""Accept as Solution""."
JBond.1
JBond.1Author
Senior
Sep 11, 2021 6:42 PM UTC

I have verified that flash is correct, currently I dont use bootloader to load the application it is loaded with keil to 0x08004000 up to 0x0801005D0. Could this be some kind of issue when the app goes to 0x08010000?

I cant step through the program, because it does not jump to the start of it, when I remove some C files it jusmps to HAL_Init as it should, I will try to remove different C files, and maybe will try to confirm if its application size or those C files are the issue.

Tesla DeLorean
Guru
Sep 11, 2021 1:36 PM UTC

It spans a flash sector boundary, perhaps you don't erase or write correctly

4x 16KB (@ 0x08000000)

1x 64KB (@ 0x08010000)

7x 128KB (@ 0x08020000)

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
JBond.1
JBond.1Author
Senior
Sep 11, 2021 6:45 PM UTC

Currently I dont use bootloader to load the application it is loaded with keil to 0x08004000 up to 0x0801005D0. So it should erase correctly. Also I have erased flash with STM32 Link utility and flashed bootloader and application, but if I try to debug application with Keil it does not hit the start of the application it jumps somewhere else. Could this be some kind of issue related that the application spans over 0x08010000 address?

Tesla DeLorean
Guru
Sep 11, 2021 6:59 PM UTC

Keil should be able to build and program.

Perhaps the BKPT comes from the use of a printf or STDIO functionality. If using the version 5 compiler, perhaps disable the semi-hosting and provide IO routines.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
JBond.1
JBond.1Author
Senior
Sep 11, 2021 7:32 PM UTC

I have changed this code:

void CheckBytes(uint16_t bytesToCheck)
{
 uint16_t bytes = MIN(64, bytesToCheck);
 uint8_t buffer[bytes];
 
 //...
}

To this:

void CheckBytes(uint16_t bytesToCheck)
{
 uint16_t bytes = MIN(64, bytesToCheck);
 uint8_t buffer[64];
 
 //...
}

And now application runs without issue. So it seems it had issue with dynamic array creation. But this code should not run on the start off the application. why it crashes on the start? Does this code requires heap memory?

Tesla DeLorean
Guru
Sep 11, 2021 7:57 PM UTC

The stack and heap sizes are described in startup.s

That would use stack space.

In the C++ case, the constructors, called prior to main(), and after SystemInit() would need dynamic memory off the heap.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..