Skip to main content
Tesla DeLorean
Guru
October 5, 2019
Question

STM32 Cube Programmer v2.1.0 not working with STM32H750B-DK QSPI External Loader

Stock hardware, and also updated with v35 ST-LINK/V3 firmware

Using MT25TL01G loader for either H750B-DISCO or H745I-DISCO External Loaders

Tried on two different machines

09:41:26 : UPLOADING ...

09:41:26 : Size : 131072 Bytes

09:41:26 : Address : 0x90000000

09:41:26 : Read progress:

09:41:31 : Error: Data read failed

09:41:51 : UPLOADING ...

09:41:51 : Size : 131072 Bytes

09:41:51 : Address : 0x90000000

09:41:51 : Read progress:

09:42:21 : Error: Data read failed

QSPI viable using my own apps, and stock demo.

Not sure the tool actually calls Init function, seen other issues where first read returns zeros, this case times out every time, never seen it read the memory.

This topic has been closed for replies.

18 replies

Tesla DeLorean
Guru
October 6, 2019
19:58:56:826 : UPLOADING ...
19:58:56:827 : Size : 1024 Bytes
19:58:56:827 : Address : 0x90000000
19:58:56:827 : Read progress:
19:58:56:827 : Reading data...
19:58:56:827 : reset ap 0
 
19:58:56:855 : halt ap 0 Status = 0
19:58:56:855 : halt ap 1 Status = 32
19:58:56:855 : halt ap 2 Status = 32
19:58:56:855 : w ap 0 reg 15 PC (0x24000000)
19:58:56:855 : w ap 0 reg 17 MSP (0x24000500)
19:58:56:856 : w ap 0 reg 16 xPSR (0x01000000)
 
19:58:56:882 : w ap 0 @0x240017E0 0x00000200 bytes
19:58:56:887 : w ap 0 @0x24000000 0x00000004 bytes
19:58:56:887 : w ap 0 @0x24000004 0x000013B8 bytes
 
19:58:56:888 : Init flashloader...
19:58:56:892 : halt ap 0
19:58:56:892 : w ap 0 reg 0 R0 0x00000000
19:58:56:892 : w ap 0 reg 1 R1 0x00000000
19:58:56:892 : w ap 0 reg 2 R2 0x00000000
19:58:56:892 : w ap 0 reg 3 R3 0x00000000
19:58:56:893 : w ap 0 reg 4 R4 0x00000000
19:58:56:893 : w ap 0 reg 5 R5 0x00000000
19:58:56:893 : w ap 0 reg 6 R6 0x00000000
19:58:56:893 : w ap 0 reg 7 R7 0x00000000
19:58:56:893 : w ap 0 reg 8 R8 0x00000000
19:58:56:894 : w ap 0 reg 9 R9 0x00000000
19:58:56:894 : w ap 0 reg 10 R10 0x00000000
19:58:56:894 : w ap 0 reg 11 R11 0x00000000
19:58:56:894 : w ap 0 reg 12 R12 0x00000000
19:58:56:895 : w ap 0 reg 13 SP 0x00000000
19:58:56:895 : w ap 0 reg 14 LR 0x24000001
 
19:58:56:895 : w ap 0 reg 15 PC 0x20000935 <<<< NOT RIGHT ADDRESS Init=0x24000935
 
19:58:56:895 : w ap 0 reg 16 xPSR 0x01000000
19:58:56:896 : w ap 0 reg 17 MSP 0x240017B8
19:58:56:896 : w ap 0 reg 18 PSP 0x00000000
19:58:56:896 : run ap 0
 
19:59:01:000 : halt ap 0
19:59:01:001 : Init function fail with timeout
19:59:01:001 : r ap 0 reg 16 xPSR 0x41000003
19:59:01:020 : reset ap 0
19:59:01:098 : halt ap 0 Status = 0
19:59:01:105 : halt ap 1 Status = 32
19:59:01:105 : halt ap 2 Status = 32
19:59:01:105 : w ap 0 reg 15 PC (0x24000000)
19:59:01:106 : w ap 0 reg 17 MSP (0x24000500)
19:59:01:106 : w ap 0 reg 16 xPSR (0x01000000)
19:59:01:106 : Error: Data read failed

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
October 6, 2019

The Command Line version also has a heap of issues.

If the External Loader exports a "Read" function, the tool doesn't bother to load the loader before executing the "Init" function.

15:58:26:328 Database: Config 6 is active.
15:58:26:328 Device name : STM32H7xx
15:58:26:332 Flash size : 128 KBytes
15:58:26:334 Device type : MCU
15:58:26:334 Device CPU : Cortex-M7
15:58:26:336
15:58:26:336 Reading data...
15:58:26:337 r ap 0 @0x1FF095F0 0x00000004 byte
15:58:26:337
UPLOADING ...
15:58:26:338 File : h7dk.bin
15:58:26:339 Size : 4194304 Bytes
15:58:26:341 Address: : 0x94000000
15:58:26:342 Read progress:
15:58:26:343 Reading data...
15:58:26:343 Loader read... <<< Doesn't actually write anything to RAM
15:58:26:343 Init flashloader...
15:58:26:344 halt ap 0
15:58:26:344 w ap 0 reg 0 R0 0x00000000
15:58:26:345 w ap 0 reg 1 R1 0x00000000
15:58:26:345 w ap 0 reg 2 R2 0x00000000
15:58:26:346 w ap 0 reg 3 R3 0x00000000
15:58:26:346 w ap 0 reg 4 R4 0x00000000
15:58:26:346 w ap 0 reg 5 R5 0x00000000
15:58:26:347 w ap 0 reg 6 R6 0x00000000
15:58:26:347 w ap 0 reg 7 R7 0x00000000
15:58:26:347 w ap 0 reg 8 R8 0x00000000
15:58:26:348 w ap 0 reg 9 R9 0x00000000
15:58:26:348 w ap 0 reg 10 R10 0x00000000
15:58:26:349 w ap 0 reg 11 R11 0x00000000
15:58:26:349 w ap 0 reg 12 R12 0x00000000
15:58:26:349 w ap 0 reg 13 SP 0x00000000
15:58:26:350 w ap 0 reg 14 LR 0x00000000
15:58:26:350 w ap 0 reg 15 PC 0x24001621
15:58:26:350 w ap 0 reg 16 xPSR 0x01000000
15:58:26:351 w ap 0 reg 17 MSP 0x00000000
15:58:26:351 w ap 0 reg 18 PSP 0x00000000
15:58:26:351 run ap 0
15:58:31:000 halt ap 0
15:58:31:000 Init function fail with timeout <<< Surprise, it fails
15:58:31:001 r ap 0 reg 16 xPSR 0x41000003
15:58:31:004 reset ap 0 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
October 6, 2019

Command Line v2.0.0, also has memory address for Init mapped at 0x20000000 vs 0x24000000 space

UPLOADING ...
16:10:41:360 File : h7dk.bin
16:10:41:362 Size : 4194304 Bytes
16:10:41:363 Address: : 0x94000000
16:10:41:364 Read progress:
16:10:41:365 Reading data...
16:10:41:368 reset ap 0
16:10:41:369 run ap 0
16:10:41:369 halt ap 0
16:10:41:369 w ap 0 reg 15 (0x24000000)
16:10:41:370 w ap 0 reg 17 (0x24000500)
16:10:41:371 w ap 0 reg 16 (0x01000000)
16:10:41:372 w ap 0 @0x240036A0 0x00000200 bytes
16:10:41:373 w ap 0 @0x24000000 0x00000004 bytes
16:10:41:391 w ap 0 @0x24000004 0x00003278 bytes <<<< Code from loader written int AXI RAM
16:10:41:391 Init flashloader...
16:10:41:391 halt ap 0
16:10:41:392 w ap 0 reg 0 0x00000000
16:10:41:392 w ap 0 reg 1 0x00000000
16:10:41:393 w ap 0 reg 2 0x00000000
16:10:41:393 w ap 0 reg 3 0x00000000
16:10:41:394 w ap 0 reg 4 0x00000000
16:10:41:394 w ap 0 reg 5 0x00000000
16:10:41:394 w ap 0 reg 6 0x00000000
16:10:41:395 w ap 0 reg 7 0x00000000
16:10:41:395 w ap 0 reg 8 0x00000000
16:10:41:395 w ap 0 reg 9 0x00000000
16:10:41:396 w ap 0 reg 10 0x00000000
16:10:41:396 w ap 0 reg 11 0x00000000
16:10:41:397 w ap 0 reg 12 0x00000000
16:10:41:397 w ap 0 reg 13 0x00000000
16:10:41:397 w ap 0 reg 14 0x24000001
16:10:41:398 w ap 0 reg 15 0x20001621 <<<< Wrong Memory
16:10:41:398 w ap 0 reg 16 0x01000000
16:10:41:398 w ap 0 reg 17 0x24003678
16:10:41:399 w ap 0 reg 18 0x00000000
16:10:41:399 run ap 0
16:10:46:000 halt ap 0
16:10:46:000 Init function fail with timeout
16:10:46:001 r ap 0 reg 16 0x81000003
16:10:46:004 reset ap 0

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
October 6, 2019

If one of the *.stldr in the ExternalLoader (QSPI NOR) lacks an "SectorErase" function the GUI tool never starts properly, you get the splash screen, but app never loads.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
October 14, 2019

@STOne-32​ @Khouloud GARSI​ 

Can someone from the STM32 Cube Programmer group please work with me to fix the tool so it works properly? The tool behaves differently with H7 targets and doesn't relocate some of the entry points properly from the .ELF/.STLDR side.

The ST-LINK Utilities (v4.5.0 GUI, v3.50 CLI) work better in this regard, the CLI seems to allow for >1MB interactions with a file.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
October 14, 2019

Another custom having more luck with Cube Programmer, and less with ST-LINK Utilities, but this build wasn't working in Cube Programmer for me either.

https://community.st.com/s/question/0D50X0000BMFyt6SQD/stm32h750vbt6-xip-qspi-flash-not-working

I'm doing work with a number of FLASH parts and loaders

https://community.st.com/s/feed/0D50X0000BSaahHSQR

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Houda GHABRI
ST Employee
October 15, 2019

​Hello Clive,

Thanks for your feedback.

This problem is already fixed in last CubeProgrammer version V2.2.0 published on ST WEB .

Can you please test an tell me if it is Ok?

Do not hesiate to contact me for furthers details.

regads,

Houda

Tesla DeLorean
Guru
October 15, 2019

Thank you, I will check this shortly.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
August 30, 2020

This continues to be a problem.

The first time it loads the .ELF it gets the Init address wrong, the second time (after disconnect/connect) it loads correctly.

This seems specific to the H7 where the STLDR are put in the 0x24000000 RAM rather than 0x20000000

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
September 9, 2020

@Houda GHABRI​ 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
December 2, 2020
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..