Skip to main content
rbenv.3
Associate III
Apr 25, 2019 7:45 PM UTC
Question

STM32 Cube Programmer API

Besides function "downloadFile", is there a way of program flash using a buffer ?

The use case is not to have a firmware file, protecting the programming phase on third parties (assembly lines, testing).

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Apr 25, 2019 7:59 PM UTC

Where would that come from? And how would it be protected if pulled into a PC?

Check Segger's stand-alone programmers

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
rbenv.3
rbenv.3Author
Associate III
Apr 26, 2019 5:09 PM UTC

The idea is to receive the firmware file encrypted from ethernet, decrypt in RAM and flash it. If I have to maintain a file,

this is a little less secure. I'm also verifying the possibility of running the STM Cube Programmer on linux (Raspberry PI) and, so

I can protect it to physical access from users.