Skip to main content
AFahr.1
Associate III
Jun 9, 2021 9:35 AM UTC
Solved

STM23L496 DFU mode, DfuSeDemo not opening, but STM32Programmer yes

Hello,

I'm trying to update a micro over DFU (USB) mode since we don't always have access to the STlink programmer.

I managed to start the unit in System Memory mode by reading a backup register at startup and jumping to system firmware if it's a certain value:

/* Jump into bootloader if backup register 1
	 * has 0xB007104D written
	 */
	if(0xB007104D == RTC->BKP1R)
	{
		RTC->BKP1R = 0x0;
 
		uint32_t JumpAddress = *(__IO uint32_t*)(SYSMEM_ADDRESS + 4);
		pFunction Jump = (pFunction)JumpAddress;
 
		SysTick->CTRL = 0;
		SysTick->LOAD = 0;
		SysTick->VAL = 0;
 
		__HAL_SYSCFG_REMAPMEMORY_SYSTEMFLASH();
 
		__set_MSP(*(__IO uint32_t*)(uint32_t)SYSMEM_ADDRESS);
		Jump();
 
		while(1);
	}

To be honest, I've seen similar flavours of the same code for this purpose.

The thing is, the unit restarts in DFU mode, at least the PC says so:

0693W00000BaUxTQAV.png 

But DfuSeDemo won't give me the option to use it:

0693W00000BaUxEQAV.png 

However, it seems that STM32Programmer works:

0693W00000BaUxjQAF.png 

Questions:

  • Can I use the STM32 programmer to update the user flash with my HEX or DFU file? But then... How do I exit DFU mode????
  • Is there a reason why DfuSeDemo doesn't work? Is there anything else I need to worry about? That one has the handy "leave DFU mode" button.

Any hints are greatly appreciated.

Cheers,

Alberto

This topic has been closed for replies.
AFahr.1
AFahr.1Best answer
Associate III
Jun 10, 2021 12:12 AM UTC

Hi all,

I just noticed that this has been solved elsewhere:

https://community.st.com/s/question/0D50X0000BI0NJhSQN/dfu-bootloader-device-not-showing-up-in-dfuse-demo

Thanks!

Cheers,

Alberto

1 reply

AFahr.1
AFahr.1AuthorBest answer
Associate III
Jun 10, 2021 12:12 AM UTC

Hi all,

I just noticed that this has been solved elsewhere:

https://community.st.com/s/question/0D50X0000BI0NJhSQN/dfu-bootloader-device-not-showing-up-in-dfuse-demo

Thanks!

Cheers,

Alberto