Skip to main content
Linas L
Senior
Sep 12, 2023 9:01 AM UTC
Solved

STLink V3 CANBUS bootloader over STM32CubeProgrammer problem

Hello,
In one of my boards I was planing to use CANBUS bootloader and STLink V3 with external canbus PHY to program MCU.

I was unable to program it, I can see STlink V3 does try to do some TX on CANBUS pin, but where is no packet available that could be decoded, just train of same duty cycle pulses.

Does any one had luck with STLink V3 and external CANBUS programming ? What I am doing wrong ?

  • Yes, I added external TCAN1462VDRBRQ1 IC for programmer, and connected to RXD and TXD pins on STLINKV3_MDOS (RX 9, TX 10pin)
  • Yes, I enabled externally TCAN1462VDRBRQ1 to be in active mode all the time
  • Yes, I placed BOOT0 pin to high level when connecting power (same pin for power and BOOT)
  • YES, STM32U585 uses PB8+PB9 as per datasheet for canbus bootloader

CANBUS_MDOS.PNGCAN_PHY.PNG

BOOT.PNG

STLink.PNG

 

This topic has been closed for replies.
Maryem
MaryemBest answer
ST Employee
Nov 27, 2023 10:57 AM UTC

Hello @Linas L,

Thanks for your feedback,

I have submitted an internal ticket addressing your request to the dev team.

Internal ticket number: 167226 (This is an internal tracking number and is not accessible or usable by customers).

I'll keep you posted.

 

Maryem.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

15 replies

Linas L
Linas LAuthor
Senior
Nov 9, 2023 10:09 AM UTC

Anyone ?

ST Employee
Nov 10, 2023 4:34 PM UTC

Hello Linas,

Not sure to get your point, but if you tried to connect directly TCAN1462VDRBRQ1 CANH & CANL pins to STM32U585 PB8 & PB9 pins it won't work. You can either connect STLink-V3MODS pins 8&9 to STM32U585 PB8 & PB9 (no need to perform a real CAN bus with a transceiver) or you have to add another CAN transceiver on STM32U585 side to go back at 3V3 level (and not stay at 5V CAN bus level with CANH & CANL)

Hope it will help.

Linas L
Linas LAuthor
Senior
Nov 10, 2023 4:40 PM UTC

Hello,
In my setup I was using normal canbus wiring, meaning:

STlinkV3 <->CANPHY≈≈≈≈≈≈≈≈≈≈≈CANPHY <->STM32U5

And I when flashed firmware on STM32 i can use canbus in my system, but when I boot STM32U5 with BOOT0 high, I can't get STM32CubeProgrammer to do anything. is there any information regarding how to do it ?

Javier1
Principal
Jan 22, 2025 2:32 PM UTC

could you share your wiring with STLNK-v3 and CANPHY?

hit me up in https://www.linkedin.com/in/javiermuñoz/
ST Employee
Nov 10, 2023 5:15 PM UTC

You can find some documentations with AN2606, AN5405 or Here.

As I'm not a software guy, I think there are also differences between CAN and FDCAN bootloaders : STLink-V3MODS is CAN bootloader compatible while U5 has a FDCAN bootloader.

Best regards,

Linas L
Linas LAuthor
Senior
Nov 10, 2023 5:19 PM UTC

In same project I already implemented UART bootloader, so I am somewhat familiar with idea how they work. Just in this case I was hoping to avoid implementing it in CANBUS, since it will always be used by STLinkV3 hardware and probably running some script, so I don't have to deal with this while have faster upload times.

I guess I will try to throw some CANBUS messages and see if I get response from it.

ST Employee
Nov 22, 2023 3:02 PM UTC

Hello Linas,

Unfortunately the STLinks V3-SET or V3MODS (based on STM32F723) won't get FDCAN bootloader because the micro inside has no FDCAN.

The new STLINK-V3PWR (based on STM32H745) could have it, but I have no idea about the date it will be available.

Associate
Apr 17, 2024 10:33 AM UTC

Hi,

 

Any update on this please? I want to use the STM32H523 in a new product design but it is going to need CAN-FD programming capability.

 

Best Regards,

Shane

Javier1
Principal
Jan 21, 2025 2:42 PM UTC

What did you end up doing? coding your own FDCan bootloader host? or downgrading to classic can?

hit me up in https://www.linkedin.com/in/javiermuñoz/
Linas L
Linas LAuthor
Senior
Jan 21, 2025 4:29 PM UTC

I tested FDCAN bootloader, and it works with my own FDCAN controller, but not programmer. This is not that hard to implement, just like UART or any other bootloader.

Question do you have tools for it.