Skip to main content
CGAUC.1
Associate II
Jun 12, 2023 12:05 PM UTC
Question

STEVAL-PLC001V1 "Core is locked up" or "The core is kept under reset"

I am currently using a STEVAL-PLC001V1 board.

I am trying to program it using CubeProgrammer. I am just trying to reprogram the demo mode at the moment.

If I program it on the board without the option "Run after programming", the download is succesfull, but nothing happens on the board. But as soon as I check the option, I have the errors "Core is locked up" or "The core is kept under reset".

I already tried to erase the chip, to connect it using the "under reset" mode, and I still have the same issue.

Did someone have the same issue before me ? How can i solve it ?

This topic has been closed for replies.