Skip to main content
JOlso.12
Associate III
Apr 11, 2022 7:38 PM UTC
Question

ST32F413 Won't Program in Cube Programmer?

I have two identical pre-production PCBs containing fresh, unprogrammed 32F413VGT micros from our distributor. One board will program just fine but CubeProgrammer says "can't erase device!" when I try to program the other board.

After first scanning the PCB for visible solder shorts and open pads, the next thing I verified was that the micro wasn't soldered into the PCB upside down. I tripped last year on this often-discussed snafu caused by the ejector dimple mimicking the pin #1 identification dot.

Other early efforts to diagnose this PCB:

--the redundant corner VDD power pins have the same (correct) voltages on both boards.

--both boards have the same ~1V signal on their V_CAP pins.

--the reset line is the same state on both.

--both unprogrammed boards draw the same IDD current, a value near zero.

Any suggestion re additional things for me to check?

Does my primary 8MHz crystal oscillator have to work in order to program a 32F micro? I think no because an operating board could have an internal RC oscillator, correct?

Should I park a 'scope probe on the SWDIO and SWCLK pins and look for identical wiggles during CubeProgrammer's efforts to program?

Thanks in advance for any help you can offer on this.

Jim

Indianapolis US

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Apr 11, 2022 8:56 PM UTC

F4 will run from internal HSI 16 MHz source until code selects otherwise

Boot loader might use PLL and external sources for USB / CAN type usage

VCAPs should be around 1.25V

NRST should be close to VDD

Check if it can read memory and/or option bytes

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Piranha
Principal III
Apr 12, 2022 10:23 PM UTC

Schematic around MCU would help. At least show/describe the NRST and BOOT0 pin connections.