Skip to main content
Associate
Aug 10, 2023 2:04 AM UTC
Solved

ST-LinkUpgrade disconnects board after opening in upgrade mode. Upgrade is unable to be clicked

Hi,

I am new to stm products and am using the STM32F4 discovery. When I run ST-LinkUpgrade I am unable to click upgrade, although I can click "opening in upgrade mode". When I do this the board just disconnects. I have used the jar file for the upgrade software as well as the programmer, although the result is the same in both cases. 

I saw a similar support message from 3 years ago but it has not been answered. I have used the jar file for the upgrade software as well as the programmer, although the result is the same in both cases. 

Thanks

This topic has been closed for replies.
Lucas TetiBest answer
Associate
Aug 11, 2023 12:49 AM UTC

Hi,

I tried doing what is done in both videos but I still get the same error. The error I often get is "Unexpect error during opening (1)" My device is disconnected whenever I run the open in update mode. When I reconnect it the same thing happens again. For context, I am running this on ubuntu in VirtualBox. 

Update: I decided to run update using the windows version of the stlink updater and it worked. 

5 replies

RhSilicon
Lead
Aug 10, 2023 4:06 AM UTC

I found this video about different chip, in the comments:

- where is that Arduino code????

- - Arduino code can be any simple code. It doesn't matter what code you use. If ST-Link is fake, it won't upload any code.

https://www.youtube.com/watch?v=cprE-aVBiAU

Lucas TetiAuthorBest answer
Associate
Aug 11, 2023 12:49 AM UTC

Hi,

I tried doing what is done in both videos but I still get the same error. The error I often get is "Unexpect error during opening (1)" My device is disconnected whenever I run the open in update mode. When I reconnect it the same thing happens again. For context, I am running this on ubuntu in VirtualBox. 

Update: I decided to run update using the windows version of the stlink updater and it worked. 

RhSilicon
Lead
Aug 11, 2023 2:47 AM UTC

If it worked with Windows it also works with Virtualbox and Ubuntu, days ago I did it, it must be a driver problem.

RhSilicon
Lead
Aug 10, 2023 4:12 AM UTC

When it asks to restart ST-Link, it means that it has to be removed from the USB port and reconnected:

https://www.youtube.com/watch?v=BIuO0SeKq_k