Question
ST_Link V3MINI and Cube programmer
- 3 replies
- 1257 views
Dear mr.
I'm having problems with my project,
Everything was working fine, but one morning I lost connection with the target unit, see attached image.
I tried this with:
Two ST_Link V3MINI (I got them directly from ST)
Three different target board STM32G071 and STM32G030.
Two different PCs.
Two USB cable.
Uninstall and install SW from ST.
My configuration is no RST wire.
One of the questions- My setting is "Soft reset" but in the log I see "HWrst reset mode".
I don't remember... maybe the problem started after the ST-Link update?
Please advise.
Regards