Skip to main content
Associate
Nov 7, 2023 1:48 AM UTC
Solved

ST-LINK,Programmer error:DEV_TARGET_CMD_ERR

hello

I used ST link to connect to stm32H743 and reported an error during the Programmer download process:"Error:ST-LINK error(DEV_TARGET_CMD_ERR)“.

But,I used j-link to connect to stm32H743 and there were no errors during the stm32IDE download process.

Can you provide some suggestions,thanks

This topic has been closed for replies.
Maryem
MaryemBest answer
ST Employee
Nov 17, 2023 8:54 AM UTC

Hello @jack-uni,

In addition to the GND, SWDIO, and SWCLK pins, you will also need to connect the VCC and NRST pins. Make sure to connect the pins correctly and use the latest version of STM32CubeProgrammer.
I apologize for the delayed response.

Maryem.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

3 replies

jack-uniAuthor
Associate
Nov 7, 2023 2:19 AM UTC

The download interface of my H743 board only has three pins: gnd, swdio, and swclk.

Do you need any other connections for ST link?

Maryem
MaryemBest answer
ST Employee
Nov 17, 2023 8:54 AM UTC

Hello @jack-uni,

In addition to the GND, SWDIO, and SWCLK pins, you will also need to connect the VCC and NRST pins. Make sure to connect the pins correctly and use the latest version of STM32CubeProgrammer.
I apologize for the delayed response.

Maryem.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Visitor II
Feb 12, 2024 8:42 AM UTC

Hi Maryem,

We are using GNd, SWDIO, SWCLK and VCC pins (only 4). And working most of the time. But sometimes, we have problems in communication, Read Protection Enabled, DEV_TARGET_CMD_ERR, etc. We were able to Erase some times but couldn't download hex file as erase failures. Is there any necessity of NRST pin to be connected. We are using ST-LINK/V2 Programmer.

D. Lenin