Skip to main content
SBarn.4
Associate II
Feb 21, 2022 8:12 AM UTC
Solved

ST-LINK firmware upgrade not sticking?

Why doesn't firmware upgrade to ST-LINK not stick?

Cube Programmer says it upgrades it successful but it doesn't do it

This topic has been closed for replies.
SBarn.4
SBarn.4Best answer
Associate II
Mar 2, 2022 9:34 PM UTC

YA, I shoulda thought of that, when I stuck it in a USB directly in my PC it worked fine, got the upgrade to work too. (it was on a hub before)

newbie mistake

Thanks for your help!

8 replies

Houda GHABRI
ST Employee
Mar 2, 2022 12:28 PM UTC

Hi @SBarn.4​ ,

can you please tell me :

  • The CubeProgrammer version used
  • The start ST-Link version
  • Which version of ST-Link is supposed to be updated to?

Houda

SBarn.4
SBarn.4Author
Associate II
Mar 2, 2022 12:52 PM UTC

Thanks for the reply

I gave up on that ST-link, I think it's a clone maybe.

I did however just buy an OEM ST-link but the latest version of cube programmer doesn't recognize it, I get the windows chime when I plug the USB in no prob.

is there some initialization or registration required?

Houda GHABRI
ST Employee
Mar 2, 2022 3:42 PM UTC

Hi @SBarn.4​ ,

Using clone of ST-Link, we cannot ensure that the update will be done correctly.

Sorry I can't help you in this case.

Houda

SBarn.4
SBarn.4Author
Associate II
Mar 2, 2022 5:56 PM UTC

I'm not asking about that.

I bought your OEM ST-Link

it isn't recognized by cube .

it's a new ST-LINK and the latest cube version.

Windows chime when I plug in the USB

Tesla DeLorean
Guru
Mar 2, 2022 7:48 PM UTC

Windows 10 or 11?

Via a hub, docking station, DELL?

Which ST-LINK? V2, V3, ST authentic for sure? Link to place of purchase.

Cable? Try others, make sure not to use charging cables, or low quality ones.

Any AV or other software or policies on the machine that might block external USB, USB MSC devices?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..