Skip to main content
Visitor II
Jun 4, 2024 9:12 AM UTC
Question

Shutting down... Exit.

 

STMicroelectronics ST-LINK GDB server. Version 7.7.0

Copyright (c) 2024, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

 

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

-------------------------------------------------------------------

STM32CubeProgrammer v2.16.0

-------------------------------------------------------------------

 

 

 

Log output file: C:\Users\faruk\AppData\Local\Temp\STM32CubeProgrammer_a16684.log

ST-LINK SN : 066EFF534871754867222516

ST-LINK FW : V2J45M30

Board : NUCLEO-F303RE

Voltage : 3.26V

SWD freq : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID : 0x446

Revision ID : Rev Y

Device name : STM32F302xE/F303xE/F398xx

Flash size : 512 KBytes

Start Address : 8000000

Device type : MCU

Device CPU : Cortex-M4

BL Version : 0x40

 

 

 

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a16684.srec

File : ST-LINK_GDB_server_a16684.srec

Size : 16.75 KB

Address : 0x08000000

 

 

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 8]

Download in Progress:

 

 

File download complete

Time elapsed during download operation: 00:00:00.928

 

 

 

Verifying ...

 

 

 

 

Download verified successfully

 

 

Shutting down...

Exit.

 

I keep getting this error. I didn't get it before, it developed suddenly. it doesn't work in my previous working codes. I made a port change, it didn't change. I did debug update, it didn't happen. I turned the computer off and on, it didn't happen. I deleted the cubeide and reinstalled it, it didn't happen. can someone help me now.

This topic has been closed for replies.

1 reply

Aziz BRIGUI
ST Technical Moderator
Jun 18, 2024 1:21 PM UTC

Hello @asda

The shutting down message signifies that the CubeProgrammer plug-in did download and verify the binary. Could you share what is the issue you're seeing with this message, are you unable to debug your application ?

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.