Skip to main content
Associate
Jul 3, 2024 2:09 PM UTC
Question

SetupSTM32CubeProgrammer-2.17.0.exe failed

I got this error message when trying to install the cube programmer:

This application was configured to use a bundled java runtime environment but the runtime is missing or corrrupted

HeinzH_0-1720015336386.png

I have started an jar file to see if my local jre is broken which is not the case. Is the jre taken from the jre folder besides the exe or from the system?

HeinzH_1-1720015437731.png

I am running windows 10 x64 and do have admin rights

Tried with earlier version as well. Failed also.

I have version 2.5.0 installed

 

This topic has been closed for replies.

4 replies

ST Employee
Jul 3, 2024 10:03 PM UTC

Hi All,

 

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.

 

Regards,

Jake

ST Support

 

Visitor II
Sep 19, 2024 9:39 AM UTC

I have the same issue, did you manage to solve it? Thanks!

STTwo-32
ST Technical Moderator
Sep 19, 2024 10:12 AM UTC

Hello @Dpasc 

I tried on my side, and I haven't any issue, please, refer to this user manual to check the requirements and follow the installation instructions: STM32CubeProgrammer software description - User manual

I also find a case solved in our community referring to a similar issue: Solved: Bundled java Runtime missing or corrupted - STMicroelectronics Community

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
HeinzHAuthor
Associate
Sep 23, 2024 7:23 AM UTC

I had success in installing version 2.13. which we had downloaded some time ago. And I was at least able to work the WBA55 board now. But still no luck with actual versions from the web.