Skip to main content
Associate
May 7, 2026 7:07 PM UTC
Solved

Setting PRODUCT_STATE to CLOSED without any password

Hi there!

First of all, thank you for taking the time to read this!!! Any input is welcome.

I'm working on a project with a Nucleo-H563ZI board, and did something quite dumb: went and set the PRODUCT_STATE to CLOSED from within some dummy FW, and now I'm stuck. I can see the FW is running (LED task is blinking), but now I can't seem to access the device through Debug Authentication to bring it back to OPEN.

closed.png

When I click on Full Regression STM32CubeProgrammer complains about "Password file not found"

markopesevski_PI_0-1778180449326.png

Which is more than logical because I did not provide one (you can see on the first image). Since I didn't set any password, I tried passing in an empty file created by running:

touch empty.bin

And then, it complains with:

empty.bin.png

Is there some way to run a regression? Or do I now have a pretty brick?

Thanks in advance!!

Aziz BRIGUI
Aziz BRIGUIBest answer
ST Technical Moderator
May 19, 2026 9:52 AM UTC

Hi @markopesevski_PI

Yes, sadly the chip is permanently locked since you need to provision a debug authentication password or certificate (When product state is provisioning) in order to be able to regress once product state is higher.

Aziz  

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

1 reply

Aziz BRIGUI
Aziz BRIGUIBest answer
ST Technical Moderator
May 19, 2026 9:52 AM UTC

Hi @markopesevski_PI

Yes, sadly the chip is permanently locked since you need to provision a debug authentication password or certificate (When product state is provisioning) in order to be able to regress once product state is higher.

Aziz  

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.