Setting BORF on STM32G041F8 bricks the processor???
- 3 replies
- 649 views
STM32CubeProg 2.19.0. STM32G041F8. MacOS 15.5. ST-Link.
I'm working on setting the brown-out rising, falling, and enable options on an STM32G041F8.
I started out by just using CubeProg to set the BOR_EN enable bit in the option bytes. Works correctly. It gives me the reaction I expected and I'm able to reconnect via CubeProg.
Next I wanted to set the BORF_LEV to something other than 3 so I can test my code. I set it to 1, hit Apply, Cube prog complains that the connection is lost and it has disconnected from the device, and now when I try and connect I just get:
17:13:46 : UR connection mode is defined with the HWrst reset mode
17:13:46 : ST-LINK SN : 31FF6A064D4E353828580643
17:13:46 : ST-LINK FW : V2J46S7
17:13:46 : Board : --
17:13:46 : Voltage : 3.31V
17:13:46 : Error: Unable to get core ID
17:13:46 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug AuthenticationNo, I did not mess with the RDP values, just BORF_LEV.
CubeProg can't unbrick it. CubeIDE gets similar results. Unfortunately, for me, I duplicated the result in another processor so I thought I'd stop and reach out.
Any ideas as to how to unlock these things?
Thanks,
Andrei (your neighbour from The Great White North)