Skip to main content
Visitor II
Mar 25, 2025 1:25 PM UTC
Question

"Run after programming" only works after *changing* the setting.

Hallo zusammen,

mir ist im STM32CubeProgrammer (GUI, v2.19.0) ein merkwürdiges Verhalten im Automatic Mode aufgefallen:

Wenn man den Haken bei "Run after programming" direkt aktiviert und dann auf „Start“ klickt, wird kein Reset ausgeführt, obwohl die Option gesetzt ist. Das Programm wird nicht neu gestartet. Wenn man schnell hintereinander viele Platinen updaten will mit Neustart des Programms ist dies hinderlich

Workaround:
Wenn man den Haken einmal entfernt und dann wieder setzt, funktioniert der Reset im Automatic Mode anschließend wie erwartet. Offenbar wird die Option intern erst korrekt übernommen, wenn sie aktiv verändert wurde.

Das Verhalten ist reproduzierbar und tritt unabhängig vom Ziel-MCU auf (getestet mit STM32L4 und ST-Link v3MINIE).

:wrench:Vorschlag:
Es wäre super, wenn das in einer der nächsten Versionen behoben werden könnte – vermutlich reicht ein Fix im Initialisierungsverhalten der GUI.

Viele Grüße
BB-RTB

 

Translation:

Hello everyone,

I noticed some strange behavior in Automatic Mode in the STM32CubeProgrammer (GUI, v2.19.0):

If you check the box for "Run after programming" directly and then click "Start," a reset is not performed, even though the option is enabled. The program does not restart. This is a hindrance if you want to update many boards in quick succession and restart the program.

Workaround:
If you uncheck the box and then recheck it, the reset in Automatic Mode works as expected. Apparently, the option is only correctly applied internally once it has been actively changed.

This behavior is reproducible and occurs regardless of the target MCU (tested with STM32L4 and ST-Link v3MINIE).

Suggestion:
It would be great if this could be fixed in one of the next versions – a fix to the GUI's initialization behavior would probably suffice.

3 replies

mƎALLEm
ST Technical Moderator
Mar 25, 2025 1:32 PM UTC

Hello @BB-RTB and welcome to the community,

The official language of this ST community is English. 

Thank your for your understanding.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Amine_Jridi
ST Technical Moderator
Apr 8, 2025 3:01 PM UTC

Hello @BB-RTB,

Could you check the reset pin and boot configuration to ensure that the MCU is booting from flash and not system memory.

Thank you,

Amine.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Jim Seymour
Senior
Apr 21, 2026 4:41 PM UTC

Thank you for this post!  I was struggling with this problem for an hour this morning and your workaround works great for me!

In case anyone at ST cares, here are the details of this bug - which really needs to be fixed.

STM32CubeProgrammer latest version (v2.22.0); programming a custom board with a STM32F030C8T6.  The old  ST-Link Utility worked fine in "Automatic Mode", but Cube Programmer does not reset my board unless I do this trick of disabling and re-enabling the "Run after programming" option.