Skip to main content
ELuca.2
Associate II
Sep 14, 2023 4:18 PM UTC
Solved

RTC initialization with STM32CubeProgrammer

Hello Community,

Is it possible to initialize and start the Real Time Clock (RTC) of the STM32U585 at the same time as the firmware and Option Bytes are installed into the MCU with STM32CubeProgrammer SFI process?

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Sep 14, 2023 4:36 PM UTC

No

Although you might be able to use an External Loader to inject and run code in the Target, that can do whatever you want it too.

Otherwise, provide some user interface via a monitor/loader type implementation in your own code that can allow for serialization, clock setting, etc in your production environment or to your support technicians, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

1 reply

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Sep 14, 2023 4:36 PM UTC

No

Although you might be able to use an External Loader to inject and run code in the Target, that can do whatever you want it too.

Otherwise, provide some user interface via a monitor/loader type implementation in your own code that can allow for serialization, clock setting, etc in your production environment or to your support technicians, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..