Skip to main content
Associate II
Sep 25, 2023 12:46 PM UTC
Question

Reprogramming of the STM32H743zi2 board

Hi,

I have erased the program in the chip by pressing erase program in the STM32Cub programmer, now the board is not working , Can you please support on this issue?

 

 

 

This topic has been closed for replies.

3 replies

Issamos
Super User
Sep 25, 2023 1:05 PM UTC

Hello @mvenkat86 

Do you have the same problem as this post. If no, could you provide more details (error notifications, screenshots, ...).

Best regards.

II 

TDK
Sep 25, 2023 1:11 PM UTC

What does not working mean here? If you erase the flash, the program isn't going to do what it used to do.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ST Technical Moderator
Sep 26, 2023 8:04 AM UTC

Hello @mvenkat86 

It is possible that you are booting from system memory! Have you changed the boot address option byte?

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL