Skip to main content
PMari.11
Associate
May 23, 2020 8:59 AM UTC
Solved

Recover STM32h745I-Disco option bytes

Hi,

I was playing around with my STM32h745I-Disco and did some tests regarding starting and stopping the CM4 from the CM7. But I accidantly messed my the option bytes up. I disabled BCM7 and BCM4 with CubeProgrammer and now the chip is not starting anymore. But I can also not connect to with the embedded ST-Link to recover the option bytes. Is there a way to get the board back to work?

Thank you and best regards

Philipp

This topic has been closed for replies.
TDK
TDKBest answer
May 23, 2020 2:41 PM UTC

Use the "STM32 ST-LINK Utility" to connect to the board using access port 3 (under Target -> Settings), then change the option bytes back.

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
May 23, 2020 2:41 PM UTC

Use the "STM32 ST-LINK Utility" to connect to the board using access port 3 (under Target -> Settings), then change the option bytes back.

"If you feel a post has answered your question, please click ""Accept as Solution""."
PMari.11
PMari.11Author
Associate
May 23, 2020 11:07 PM UTC

Thank you very much this fixed my issue.