Skip to main content
Fate1
Associate II
Dec 8, 2019 7:16 AM UTC
Question

reading flash memory

Hi, with stm32cubeprogrammer i've read flash memory, but when i want to program the micro with the file that i've read, it says that "core is locked up". what should i do to solve this problem?

This topic has been closed for replies.

3 replies

S.Ma
Principal
Dec 8, 2019 9:00 AM UTC

Maybe you copied too much of the flash and the user area is smaller?

Tesla DeLorean
Guru
Dec 8, 2019 3:49 PM UTC

What part?

Is the problem with READING or WRITING (Programming)?

What memory area are you accessing?

Perhaps post a log? Select the highest debug level.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Fate1
Fate1Author
Associate II
Dec 9, 2019 11:12 AM UTC

By reading i have no problem. In "Device memory" window there is a address bar, data size and data width, that i use the default value for them. Then i choose "save as" and then read command.

By writing i receive these messages:

'Start operation achieved successfully'

'Warning : The Core is locked up'

'Download verified successfully'

'File download complete'

I'm trying to read flash memory.

What do you mean by 'post a log'? I don't understand.