Skip to main content
MGogr.1
Senior
Jul 2, 2025 4:13 AM UTC
Question

Program bin file from Cube Programmer

I have two stm32f429 Discovery boards. I programmed one of the board using cube ide; the output of which was as expected. Then using cube programmer I read and saved the bin file from that board. Using that bin file I programmed my another board which was successful, but there was no output.

Is there any another method to do this?

I am doing this because I want to save bin file from my custom board and program it to another board and I don't have original code.

This topic has been closed for replies.

8 replies

KnarfB
Super User
Jul 2, 2025 5:16 AM UTC

Besides the flash, there is also the user/option bytes area. You may want to compare those with STM32CubeProgrammer. 

Otherwsie, if you save the *entire* flash as .bin, the boards shall behave identically.

The only exception is if the firmware actively works against that, like by evaluating the unique device id etc..

hth

KnarfB

MGogr.1
MGogr.1Author
Senior
Jul 2, 2025 5:24 AM UTC

I compared  both the files and it says no difference found. But no output in second board.

Tesla DeLorean
Guru
Jul 2, 2025 5:40 AM UTC

Same model / build / revision of STM32F429I-DISCO ? Not a DISC1 ?

>>But no output in second board.

Screen? Or USART/VCP ?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
Jul 2, 2025 5:37 AM UTC

So probably not recovering and writing enough. There's 2MB of FLASH, so 0x08000000 to 0x081FFFFF

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..