Skip to main content
PieterInHetBos
Associate II
Mar 29, 2023 4:06 PM UTC
Solved

Problem with STM32G0B0: failed to download Segment[0]

I have a Nucleo board with a new MCU, base board is the Nucleo-G070RB. Now it is a ST link with a STM32G0BORE.

I have a problem with the internal bootloader where i cannot upload a new program via USB DFU.

There is no hardware problem because VCP works just fine. No data corruption of something.

I have tried .HEX .BIN and .ELF all have the same problem.

This is the error log is have:

18:04:57 : UR connection mode is defined with the HWrst reset mode

 18:04:57 : USB speed  : Full Speed (12MBit/s)

 18:04:57 : Manuf. ID  : STMicroelectronics

 18:04:57 : Product ID : DFU in FS Mode

 18:04:57 : SN     : 204E315A4630

 18:04:57 : DFU protocol: 1.1

 18:04:57 : Board    : --

 18:04:57 : Device ID  : 0x0467

 18:04:57 : UPLOADING OPTION BYTES DATA ...

 18:04:57 :  Bank     : 0x00

 18:04:57 :  Address    : 0x1fff7800

 18:04:57 :  Size     : 68 Bytes

 18:04:57 :  Bank     : 0x01

 18:04:57 :  Address    : 0x1fff7870

 18:04:57 :  Size     : 4 Bytes

 18:04:57 : UPLOADING ...

 18:04:57 :  Size     : 1024 Bytes

 18:04:57 :  Address    : 0x8000000

 18:04:57 : Read progress:

 18:04:57 : Data read successfully

 18:04:57 : Time elapsed during the read operation is: 00:00:00.031

 18:05:05 : Memory Programming ...

 18:05:05 : Opening and parsing file: g0b0test.hex

 18:05:05 :  File     : g0b0test.hex

 18:05:05 :  Size     : 42.56 KB 

 18:05:05 :  Address    : 0x08000000 

 18:05:05 : Erasing memory corresponding to segment 0:

 18:05:05 : Not flash Memory : No erase done

 18:05:05 : File segment @0x08000000 is not 255-bytes aligned. It will be aligned to @0x07FFFFF8

 18:05:05 : Download in Progress:

 18:05:05 : Error: failed to download Segment[0]

 18:05:05 : Error: failed to download the File

 18:05:05 : RUNNING Program ... 

 18:05:05 :  Address:   : 0x08000000

 18:05:05 : Start operation achieved successfully

 18:05:06 : Warning: Connection to device 0x467 is lost

 18:05:06 : Disconnected from device.

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Feb 2, 2024 1:09 PM UTC

Hi @PieterInHetBos,

Can you please check Option Byte setting?

Try this workaround: Force to erase 'entire flash' memory, before start debugging.

Can you please share the Option Bytes parameters and the log file, in order to investigate the issue.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

15 replies

ST Technical Moderator
Mar 30, 2023 2:46 AM UTC

Hello @PieterInHetBos​ and welcome to the Community :)

Could you please try to use STM32CubeProgrammer on standalone.

Make sure to use latest release of CubeProgrammer, and try to upgrade ST-LINK firmware.

Check the registers and ensure that “flash empty�? is not causing such issue.

I advise you to erase the flash memory first.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Piranha
Principal III
Mar 30, 2023 4:56 AM UTC

A code, which expects a 255-byte alignment, is definitely broken:

https://community.st.com/s/question/0D53W00002CMICqSAP/stm32cubeprogrammer-213-bugs

Mar 30, 2023 7:43 AM UTC

Hi Imen,

It seems that the 0x467 loader is really broken. The bigger problem is that CubeIDE is also relying on it to load the program before debugging, and it is now impossible on some of the G0 devices.

This must be fixed as soon as possible...

Best regards,

Kraal

ST Technical Moderator
Apr 5, 2023 7:16 AM UTC

Hi @Kraal​, Hi @PieterInHetBos​ ,

Our team is very aware of this issue now and working to fix this in the coming release.

An internal ticket ID 149042 is submitted in order to improve the tool.

(PS: ID 149042 This is an internal tracking number and is not accessible or usable by customers).

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
PieterInHetBos
Associate II
Apr 18, 2023 7:15 AM UTC

Dear Imen,

Any luck on a update?

ST Technical Moderator
Apr 18, 2023 9:24 AM UTC

Hi @PieterInHetBos​ ,

The fix is integrated and will be published in the STM32Cubeprogrammer v2.14.0.

But, for the moment I can't give you any information about delivery date.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
Feb 2, 2024 1:17 PM UTC

Hi @PieterInHetBos, 

Please share the log file and which board used.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
PieterInHetBos
Associate II
Feb 2, 2024 1:27 PM UTC

Hi @Imen.D 

I could not repoduce the issue so i am sure it was a skill issue