Skip to main content
DPark.7
Associate
Mar 17, 2023 5:07 PM UTC
Solved

Problem with "Run after programming" in CubeProgrammer with UART connection

My Settings : 

STM32G070 mit BootLoader protocol version: 3.1

STM32CubeProgrammer v2.13.0

My plan :

flash my file via UART(USART2) and my MCU should start automatically after programming is finished. I will reset the nBOOT0 bit in my programm, after my own evaluation.

My result :

I tried with "Run after programming" in CubeProgrammer and "Go 0x800000" in STM32_Programmer_CLI. In both case, downloading was successfull but MCU could not start.

See attached log file : logCP_uart.log

Step 1 : nBOOT0 = 0, nBOOT1 = 1, nBOOT_SEL = 1 : this combination by Stm32G070 leads to boot from System memory (Bootloader)

Step 2 : I could access boot loader via uart (com16) and start programming.

Step 3 : My Transmitter.elf file was downloaded (line 32) and the Verifying was also successfully (line 36).

Step 4 : But the RUNNING Program from Address 0x08000000 (line 37 and 38) could not be executed. Error Message : Error: GETID command not acknowledged! (line 44)

See attached log file : logCP_CLI.txt

Log file says, that RUNNING Program was a success. But my MCU has not started.

See attached log file : logCP_swd.log

Test to compare:

I chose SWD instead of UART. In this case, the task could be executed without any problem.

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Mar 17, 2023 5:15 PM UTC

Some STM32 need power cycling after programming

Check if the watch-dog is running, you're code may run, but you'll still have to kick it.

Has it really not started? Toggle GPIO very early in Reset_Handler

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Mar 17, 2023 5:15 PM UTC

Some STM32 need power cycling after programming

Check if the watch-dog is running, you're code may run, but you'll still have to kick it.

Has it really not started? Toggle GPIO very early in Reset_Handler

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
DPark.7
DPark.7Author
Associate
Mar 17, 2023 5:56 PM UTC

A Great Thank for Your speedy help.

I've tried with toggling GPIO before the main starts.

Yes, my MCU has toggeled !

Now I have found out, one of our function has blockt the init process, which we have packed in startup_stm32xxx.s file. I must figure out, why this makes problem.

But my problem i have posted is solved!!!

Thanks a lot for your help!